PowerLogic T300 - Clock synchronization of IEDs on the internal LAN port?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - Clock synchronization of IEDs on the internal LAN port?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Related Products
product field
Schneider Electric
PowerLogic T300

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
milica_dukic_
Ensign milica_dukic_
Ensign

Posted: ‎2023-07-24 03:43 AM . Last Modified: ‎2025-01-24 01:00 AM

0 Likes
3
1831
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
‎2023-07-24 03:43 AM

PowerLogic T300 - Clock synchronization of IEDs on the internal LAN port?

Dear all,

 

I have a question regarding the possibily to use PowerLogic T300 to synchronize the clock of local IEDs.

After configurating the IP address of an IED as 192.168.0.4 and the SNTP server as 192.168.0.254, I connect the IED to the second Ethernet LAN port of the 3rd SC150 module (the last module of my T300 hardware configuration). It synchronized but then it losts communication over IEC61850.

 

My questions are:

  1. Do I need to configure an IP address of IED to be in the same range as LAN port, or could the IP address be from a different range?
  2. On which Eternet port do I need to connect the IED (LAN or WAN)?
  3. What else needs to be set up?

 

Thanks in advance.

 

Best regards,
Milica Dukic

 

 

  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Labels
  • Labels:
  • IEC61850
  • PowerLogic T300
Tags (4)
  • Tags:
  • english
  • PowerLogic T300
  • sntp
  • t300
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
TomBerry
Lieutenant JG TomBerry Lieutenant JG
Lieutenant JG

Posted: ‎2023-07-25 12:34 AM . Last Modified: ‎2025-01-24 01:20 AM

0 Likes
1
1807
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
‎2023-07-25 12:34 AM

IEDs should be connected to the ETH1 WAN port of the HU250 module (and not to SC150, SC160 or LV150 modules).

Then the IED should be configured to get time synchronization from a router, or via SNTP from the HU250 module using HU250's WAN IP address.

 

HU250 LAN port (subnetwork 192.168.0.x) is strictly reserved for internal communications with SC150, SC160 and LV150 modules (see T300 user manual page 26 - chapter: "T300 Internal Architecture")

See Answer In Context

Reply
Replies 3
TomBerry
Lieutenant JG TomBerry Lieutenant JG
Lieutenant JG

Posted: ‎2023-07-25 12:34 AM . Last Modified: ‎2025-01-24 01:20 AM

0 Likes
1
1808
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
‎2023-07-25 12:34 AM

IEDs should be connected to the ETH1 WAN port of the HU250 module (and not to SC150, SC160 or LV150 modules).

Then the IED should be configured to get time synchronization from a router, or via SNTP from the HU250 module using HU250's WAN IP address.

 

HU250 LAN port (subnetwork 192.168.0.x) is strictly reserved for internal communications with SC150, SC160 and LV150 modules (see T300 user manual page 26 - chapter: "T300 Internal Architecture")

Reply
milica_dukic_
Ensign milica_dukic_
Ensign

Posted: ‎2023-07-26 06:01 AM

0 Likes
0
1792
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
‎2023-07-26 06:01 AM

Thanks Tom.

 

Best regards, Milica

Reply
John_Archer1
Ensign John_Archer1
Ensign

Posted: ‎2024-10-28 03:16 AM

0 Likes
0
1027
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
‎2024-10-28 03:16 AM

Hello Tomberry, I can't adjust the time of the computer that is monitoring the scada system using the NTP protocol of the T300. Please let me know about this.

T300 Can a normal computer be set to synchronous time?
SCADA is able to adjust the timing of other relays connected to the system.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.