Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

PowerLogic T300 - Smart RM6: sharing LPVT connection for revenue meter

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - Smart RM6: sharing LPVT connection for revenue meter
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Commander Araceli_Monje Commander
43
Arun-kumar_PS
Commander Arun-kumar_PS Commander
21
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Protection & Control
Start a Topic
sesa122761_brid
Lieutenant JG sesa122761_brid Lieutenant JG
Lieutenant JG

Posted: ‎2021-07-27 08:39 AM . Last Modified: ‎2025-05-26 12:42 AM

0 Likes
4
1789
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
‎2021-07-27 08:39 AM

PowerLogic T300 - Smart RM6: sharing LPVT connection for revenue meter

Dear All ,

 

One of our Smart RM6 customers would like to share the existing LPVT voltage sensors (going to PowerLogic SC150 module) with a Revenue Meter. Is that possible and if yes, how?

 

Thanks in advance 

Attachments
Labels
  • Labels:
  • Application cases
  • PowerLogic T300
Tags (5)
  • Tags:
  • english
  • LPVT
  • PowerLogic T300
  • revenue meter
  • Smart RM6
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 4
Juha
Captain Juha Captain
Captain

Posted: ‎2021-08-03 06:32 AM

1 Like
0
1780
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
‎2021-08-03 06:32 AM

Hi @sesa122761_brid , 

 

LPIT's (Low Power Instrumentation Transformers) can not be paralleled like 
traditional instrumentation transformer. It requires an amplifier to distribute the

LPIT signal for several devices.

 

BR

 

-juha-

Tags (1)
  • Tags:
  • english
Reply
JYPOC
Commander JYPOC Commander
Commander

Posted: ‎2021-08-03 06:59 AM . Last Modified: ‎2021-08-03 07:12 AM

1 Like
2
1775
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
‎2021-08-03 06:59 AM

Hi,

 

We investigated a few years ago and it was deemed possible to connect up to 3 or 4 Easergy SC150-VT/LPVT modules to a single LPVT output. However, this has not been tested with other products: hence the solution provided (i.e. to use a LPVT sharing hub) will probably be needed to add this revenue meter.

 

Note: the RM6 is fitted with 3 LPVTs (Class 0.5) and 3 RM6 bushing CTs (Class 0.5). This is why the Easergy T300 provides a Power Measurement at Class 1.

 

If the revenue meter is connected to the same current/voltage sources, it cannot provide a Power Measurement better than Class1: so what is the idea here???

BR - Jean-Yves
  • Thumbnail of PowerLogic T300
    Schneider Electric
    PowerLogic T300
View products (1)
Tags (4)
  • Tags:
  • easergy t300
  • english
  • LPVT
  • RM6
Reply
sesa122761_brid
Lieutenant JG sesa122761_brid Lieutenant JG
Lieutenant JG

Posted: ‎2021-08-08 01:59 AM . Last Modified: ‎2021-08-13 01:42 AM

0 Likes
1
1768
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
‎2021-08-08 01:59 AM

Thank you very much.

 

Do we know the type of 'LPVT sharing hub' in the market  that could be used in this case ?

It looks to me any case with the existing LPVT type we use in RM6 , it is not possible to use external additional revenue meter beside SC150 since the accuracy for the meter will not be achieved except customer accepts with some tolerance on the accuracy for the meter  ? 

Tags (1)
  • Tags:
  • english
Reply
JYPOC
Commander JYPOC Commander
Commander

Posted: ‎2021-08-13 01:59 AM

0 Likes
0
1758
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
‎2021-08-13 01:59 AM

  1. What LPVT hub can we use?
    • Since this has never been tested, I cannot recommend any.
    • I have found this reference on internet so I suggest you purchase one to test it (https://in.rsdelivers.com/product/rs-pro/21993050-50/rs-pro-cat5e-rj45-t-adapter-2-port-shielded-170...).
    • We ourselves plan to acquire some units to also do the test in Technopole/ Grenoble (FR)
  2. Sharing Smart RM6 bushing current transformers?
    • To perform revenue metering on the MV side, your revenue meter will need to connect to CTs.
    • What do you intend to do: add another set of 3 CTs on the MV feeder, or share the existing ones?
      • The Smart RM6 is not designed to share the output from the 3 bushing CTs (1 A, 500/1).
      • In addition, opening the secondary side of 1 A CTs cannot be performed on a live line (meaning: you will need to switch off the MV on the RM6 bushing)

 

And as I said before, a Revenue Meter can provide a high accuracy on the complete chain when it is directly connected to the voltage (which is the case for LV measurement) and CTs with a Class better than 0.5. . But it won't be the case here as LPVT is Class 0.5 and RM6 bushing CT is Class 0.5.

 

BR - Jean-Yves
Tags (1)
  • Tags:
  • english
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.