Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Saitel DP/ Saitel DR/ PowerLogic T300 - blocking remote command from upper lvl SCADA?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • Protection & Control
  • Saitel DP/ Saitel DR/ PowerLogic T300 - blocking remote command from upper lvl SCADA?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
41
Arun-kumar_PS
Arun-kumar_PS Mentor
33
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
Back to Protection & Control
Start a Topic
Solved
Ivan_Puškaš_EC
Ivan_Puškaš_EC
Troubleshooter

Posted: ‎2021-08-12 12:26 AM . Last Modified: ‎2024-07-05 01:23 AM

0 Likes
1
1686
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
‎2021-08-12 12:26 AM

Saitel DP/ Saitel DR/ PowerLogic T300 - blocking remote command from upper lvl SCADA?

Hi everyone,

 

As one of the solutions, we use Saitel DP as an RTU for MV SS.

Ad its normal features:

* getting information from relays over communication  (IEC61850 most common);

* information by DI/DO/AI ;

* sending these information to the upper level SCADA system by protocol ;

* receiving commands from upper level SCADA. (IEC101, IEC104...) ;

 

And now we get to the main point. There is need that in some conditions like when main local/remote switch in SS is in LOCAL state, all the  commands from upper level SCADA that comes to Saitel should be blocked and/or not executed. Example: SCADA sends over IEC104 command to Saitel, and Saitel sends over IEC61850 open/close command to IED

 

So we have lets say digital input wired on Saitel that signals that main local/remote switch is in LOCAL, and we need to block remote commands  that comes  to the Saitel and/or to be executed to the IED.  

 

Anyone done similar thing or any idea witch signal in Saitel can be used for this?

 

Similar thing can be for Saitel DR, or even maybe T300, as they are on same platform/software,

 

Best regards,

Labels
  • Labels:
  • PowerLogic T300
  • Saitel range
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
AndreMelo
AndreMelo Mentor
Mentor

Posted: ‎2021-08-12 12:35 AM

1 Like
0
1684
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
‎2021-08-12 12:35 AM

hi @Ivan_Puškaš_EC 

 

In status table:

 

  GECC02_GATE_SUBST_MODE SUBSTATION MODE Formula GECC02_GATE_SUBST_CMD   TSGTW01 [TSGTW01SYSTEM/LLN0$ST$RemLoc$]stVal:q:t             1 False False False False

 

in cmd table:

  GECC02_GATE_SUBST_CMD SUBSTATION MODE COMMAND TSGTW01 [TSGTW01SYSTEM/LLN0$CO$RemLoc$] SCADA 200296:CSC     Formula GECC02_GATE_SUBST_MODE:EVENT SOE GECC02_GATE_SUBST_CMD:YES     False

 

Where:

 

SCADA is the 104 channel

TSGTW01 is the saitel it-self.

 

Best Regards

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Reply 1
AndreMelo
AndreMelo Mentor
Mentor

Posted: ‎2021-08-12 12:35 AM

1 Like
0
1684
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
‎2021-08-12 12:35 AM

hi @Ivan_Puškaš_EC 

 

In status table:

 

  GECC02_GATE_SUBST_MODE SUBSTATION MODE Formula GECC02_GATE_SUBST_CMD   TSGTW01 [TSGTW01SYSTEM/LLN0$ST$RemLoc$]stVal:q:t             1 False False False False

 

in cmd table:

  GECC02_GATE_SUBST_CMD SUBSTATION MODE COMMAND TSGTW01 [TSGTW01SYSTEM/LLN0$CO$RemLoc$] SCADA 200296:CSC     Formula GECC02_GATE_SUBST_MODE:EVENT SOE GECC02_GATE_SUBST_CMD:YES     False

 

Where:

 

SCADA is the 104 channel

TSGTW01 is the saitel it-self.

 

Best Regards

Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.