Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Easergy P5F30 Issue connection fall after 5-7 min. with Easergy Setup Via Ethernet USB

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • Protection & Control
  • Re: Easergy P5F30 Issue connection fall after 5-7 min. with Easergy Setup Via Ethernet USB
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
41
Arun-kumar_PS
Arun-kumar_PS Mentor
33
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
Back to Protection & Control
Start a Topic
Solved
PaterninaEnriqu
PaterninaEnriqu Explorer
Explorer

Posted: ‎2021-05-28 08:17 AM . Last Modified: ‎2023-05-30 10:07 PM

0 Likes
3
2163
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
‎2021-05-28 08:17 AM

Easergy P5F30 Issue connection fall after 5-7 min. with Easergy Setup Via Ethernet USB

Good morning.

 

I am writing to detail a problem that is happening to us with the Easergy P5F30 that we have mounted in SAT tests for some 69kV line boards integrated into IHM Ecosui. 

 

Problem description

Loss of connection with Easergy Setup via Ethernet and via USB (front panel). The equipment does not allow management through any of its ports. It only allows a temporary connection with the Easergy P5F30 in both ports for about 5-7 min after restarting the equipment (turning off and power on the power supply).

 

Observations

  • The device shows blocking of the connection with the Easergy Setup, however, it allows pinging the device through the Windows CMD.
  • The equipment does not present blocking of 61850 signals on the network: there is no evidence of loss or unknown signals, programmed in the Ecosui event window.
  • We have twelve (12) P5F30s with different settings and the same behavior occurs in all.
  • On the same network, we have a P3T32 and it has normal behavior. There are no connection problems with the Ecosui, or with the Easergy Setup.
  • We need permanent monitoring in all the equipment involved in the control system (IED / HMI / Gateway / Clients and SCADA simulators ...) in the SAT tests

 

Procedures performed by on-site technician

  • Management test with different PCs: In order to rule out problems with the PC ports, the same problem was presented on four (4) different PCs (two of them without Schneider's internal IT policies) and the same behavior. Therefore PC problems are ruled out.
  • Easergy Setup version change: Tested with two of the latest versions of Easergy Setup 3.0.0 and 3.0.1./3.1.1/3.2.0 The same problem occurs.
  • Restarting P5F30 units: temporarily solved by recovering the Easergy Setup management connection via USB and Ethernet for about 5-7 min. After this time, it does not allow connection to the Easergy Setup.
  • Firmware V300.103 and The firmware comes with Basic CS.

 

P5F30 Basic CS.png

 

I am open for any comments or suggestions for the resolution of this issue.

  • Thumbnail of PowerLogic P3
    PowerLogic
    PowerLogic P3
View products (1)
Labels
  • Labels:
  • Application cases
  • PowerLogic P5
Tags (2)
  • Tags:
  • Ecosui IHM eSetup
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
AndreMelo
AndreMelo Mentor
Mentor

Posted: ‎2021-05-28 10:30 AM

0 Likes
0
2150
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
‎2021-05-28 10:30 AM

@PaterninaEnriqu 

 

We were in V01.300 and we update to V01.303.

 

BR

See Answer In Context

Tags (1)
  • Tags:
  • english
Reply
Replies 3
AndreMelo
AndreMelo Mentor
Mentor

Posted: ‎2021-05-28 08:37 AM

0 Likes
2
2160
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
‎2021-05-28 08:37 AM

@PaterninaEnriqu 

 

I had a similar issue last week, however, it was happening when the relay got synchronized via SNTP.  please check that.

 

In this case the solution was the firmware upgrade, please check that and contact your local support.

 

Best Regards 

Tags (1)
  • Tags:
  • english
Reply
PaterninaEnriqu
PaterninaEnriqu Explorer
Explorer

Posted: ‎2021-05-28 08:50 AM . Last Modified: ‎2021-05-28 08:52 AM

0 Likes
1
2156
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
‎2021-05-28 08:50 AM

Thanks for the answer. The Synchronization is OK via SNTP. We test without the GPS and the issue persist.¿Do you know the firmware version upgraded/downgraded?

 

Synch P5.png

 

Tags (1)
  • Tags:
  • english
Reply
AndreMelo
AndreMelo Mentor
Mentor

Posted: ‎2021-05-28 10:30 AM

0 Likes
0
2150
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
‎2021-05-28 10:30 AM

@PaterninaEnriqu 

 

We were in V01.300 and we update to V01.303.

 

BR

Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.