Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

electrical & mechanical spec and EMC test of IM400

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • electrical & mechanical spec and EMC test of IM400
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Anonymous user
Not applicable

Posted: ‎2015-04-10 07:08 AM . Last Modified: ‎2020-04-20 06:09 AM

0 Likes
0
959
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
‎2015-04-10 07:08 AM

electrical & mechanical spec and EMC test of IM400

Below is L4's response to one internal customer (DCN) question, it is about the electrical and mechanical spec and EMC test levels of IM400:

 

- Les tenues aux chocs (The shock voltage)
Generic Standard           EN 60068-2-27
Severity                         15 g / 11 ms (catégorie 3M4 de la IEC 60721-3)

 

- Tenues aux vibrations (The tolerance to vibration)

Generic Standard             IEC 60068-2-6 and IEC 61557-1   IACS E10 §7
Standards                       IEC 61557-1   IACS E10 §7
Severity                          1 g / 3,5 mm (catégorie 3M4 de la IEC 60721-3)

 

- Tenues CEM

attached PDF.

Attachments
Labels
  • Labels:
  • Insulation Monitoring
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.