Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

What are the defenses we have for relay+meter 2 in one competition

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • What are the defenses we have for relay+meter 2 in one competition
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Anonymous user
Not applicable

Posted: ‎2014-08-04 06:45 PM

0 Likes
2
1164
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
‎2014-08-04 06:45 PM

What are the defenses we have for relay+meter 2 in one competition

Hi

I have seen relay+meter products in projects.

End users and consultants have the impression that it must be cheaper with the combined product.

However, I want to know technically, what is the benefit of separating these two functions instead of one?

So I can tell them that they're probably saving money at cost of system reliability... bla bla bla...


Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Yut
Yut
Leader

Posted: ‎2014-08-07 01:39 AM

1 Like
0
1129
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
‎2014-08-07 01:39 AM

Relay always connects to higher saturate point CT but less accurate while meter always connects to high accuracy CT at its rated value giving more accurate reading.

Reply
sesa50168
sesa50168 Leader
Leader

Posted: ‎2014-08-07 07:39 AM

3 Likes
0
1129
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
‎2014-08-07 07:39 AM

Typically, the relay CTs do not have the same level of accuracy that metering CTs have, as Yut mentioned.  The specific metering need will drive the decision of discrete metering or protection + metering.  If the customer only wants basic metering, and not concerned about accuracy and power quality, then influence the customer to use Schneider relays that have the metering functionality.   If it is a revenue meter application, I would expect the customer to prefer separate metering, since the meter is the customer's cash register.  Has the relay received third party accuracy certification?  Likely not.   A device that is specifically designed for metering is the best choice in a critical application, as opposed to using a secondary function (metering) of a protective device.  Looking at it from the other direction, our meters could, in theory, be used as protective devices, but they are not used that way because it is not the primary function of the device.  The same philosophy applies to using protective relays for metering.  Use the right device for the right application.

The point is power quality.  I've not heard of a protective relay having certified compliance with IEC 61000-4-30 Class A, which our meters have.  Relays typically have slower sample rates, and therefore poorer waveform capture capability.  Also keep in mind that our meters can compensate for transformer losses, so they can be placed on the transformer secondary, where the CTs and PTs will be much less expensive.  Our meters are designed for PQ applications including sag/swell and transient detection and waveform capture, and harmonic analysis.  Like the revenue metering situation, if power quality is a concern, it is best to use the device designed for that application.  Fortunately, we have successfully combined revenue and PQ metering into a single device.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.