Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84257members
353353posts

Reverse engineering transformer and line loss

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

alister_brunsde
Lt. Commander
Lt. Commander
0 Likes
1
353

Reverse engineering transformer and line loss

Hi all,

A default ION 7/8000 series meter has frameworks for calculating transformer and line losses. If there is an error in the loss parameters and the meter goes into service, the uncompensated values are not logged anywhere. Since the incorrect compensated values must be corrected; does anyone have a method/spreadsheet to handle this scenario? I assume by reverse engineering the loss formulas with an assumed steady voltage, pf etc the amperage for each interval energy value can be derived?

Any thoughts greatly appreciated.

1 Reply 1
sesa46696_bridg
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
301

Re: Reverse engineering transformer and line loss

We have a number of customers that will modify their framework to record both compensated and uncompensated values, seems a bit safer if they program the meter incorrectly. Many customers will just do the compensation in MV90 rather than the meter.