Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello,
I received following inquiry from a customer, but I don't have old PQM so I would like some advice.
As a general rule, I understand that older PQMs will need to have their firmware updated in stages.
ex, ION9000:v2.0.0 ⇒ v2.1.0 ⇒ v2.2.1 ⇒ V4.6.0
However, what happens if you accidentally upgrade the firmware from V2.0.0 to V4.6.0?
Will an error occur during the update and all operations will be canceled?
Or will the update go through to completion and the measurements become abnormal?
Best regards,
Miyai
Link copied. Please paste this link to share this article on your social media post.
Hi @Miyai
Firmware version V2.1.0 acts as an upgrade agent, as it is the minimum required version to proceed with an upgrade to the lates ones. Once the meter is updated to V2.1.0, it can be directly upgraded to the latest version (V4.6.0) without needing to go through V2.2.1.
The upgrade path is: V1.4.3 -> V2.1 -> V3.1 or V4.0.0 or V4.5.0 or V4.6.0(which is the latest) as long as firmware version 2.1.0 have been previously installed and ensure using the latest version of Install ION Setup when upgrading to V4.6 (v3.2.25037.01 or higher). The current version is v3.2.251185.01 .
The upgrade process will fail during validation, and the meter will reject the firmware file because existing firmware versions earlier than V2.1.0 do not support upgrades to later versions.
No changes will be made to the meter, and it will remain on its current firmware version. Since the firmware is not applied, no abnormal measurements or data corruption should occur.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hello Mehran,
Note that ION9000 meters did not have a V1.4.3, the ION9000 meters started with V2.0.0. You are correct that V2.1.0 is a requirement before upgrading to any later versions of firmware.
@Miyai if you try to upgrade a meter with V2.0.0 firmware, the meter will reject the latest firmware file as the meter does not understand the file format.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hi @Miyai
Firmware version V2.1.0 acts as an upgrade agent, as it is the minimum required version to proceed with an upgrade to the lates ones. Once the meter is updated to V2.1.0, it can be directly upgraded to the latest version (V4.6.0) without needing to go through V2.2.1.
The upgrade path is: V1.4.3 -> V2.1 -> V3.1 or V4.0.0 or V4.5.0 or V4.6.0(which is the latest) as long as firmware version 2.1.0 have been previously installed and ensure using the latest version of Install ION Setup when upgrading to V4.6 (v3.2.25037.01 or higher). The current version is v3.2.251185.01 .
The upgrade process will fail during validation, and the meter will reject the firmware file because existing firmware versions earlier than V2.1.0 do not support upgrades to later versions.
No changes will be made to the meter, and it will remain on its current firmware version. Since the firmware is not applied, no abnormal measurements or data corruption should occur.
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hello Mehran,
Note that ION9000 meters did not have a V1.4.3, the ION9000 meters started with V2.0.0. You are correct that V2.1.0 is a requirement before upgrading to any later versions of firmware.
@Miyai if you try to upgrade a meter with V2.0.0 firmware, the meter will reject the latest firmware file as the meter does not understand the file format.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello, @Charles_Murison , @Mehran_Mehrnia
Thank you for your advice.
I will explain to customer.
Best regards,
Miyai
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.