Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84729members
354149posts

Reboot ETH Card ION8650C

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

MarthaV
Lt. Commander
Lt. Commander
0 Likes
1
211

Reboot ETH Card ION8650C

Hello

I have a case where clients are changing the ETH communication through modem to direct LAN connection with some ION8650C,

after two changes, the meter was connected and then dropped the connection and it didn't get connect till they reboot the meter,

Why could be this happening?, and if there a way to reboot remotely only the ETH Card a second before the exchange?, since there are no able to reboot all the meters.

Martha

1 Reply 1
sesa82206
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Reboot ETH Card ION8650C

Hello Martha,

I have seen similar behavior with other meters as well when PoE (Power over Ethenet) is enabled.

Regards,