Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

RD96 on PM8000 Downloading Error

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • RD96 on PM8000 Downloading Error
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
529
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
140
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
dsantillan
Lieutenant dsantillan
Lieutenant

Posted: ‎2023-08-29 08:02 AM

0 Likes
5
2566
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
‎2023-08-29 08:02 AM

RD96 on PM8000 Downloading Error

Hello, 

 

We recently installed a PM8244 meter with RD96 display. 

 

PM8000 firmware 004.000.000

 

Upon connection of the RD96 the screen reads Downloading Application 004 003 007

After a few minutes it changes to Downloading Error and the Display cannot be operated. 

 

How can this be corrected?

 

Thank you. 

 

 

 

 

Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-08-30 07:59 AM

0 Likes
1
2524
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
‎2023-08-30 07:59 AM

Hello @dsantillan ,

 

When you connect to the meter with ION Setup or PME, there is a module called Factory. One of the output registers of this module is RMD serial number and RMD version. If the meter does not have this information it indicates that meter is not able to talk to the display.

 

The "system" has 3 parts, the meter, the display and the cable between display and meter. Hard to say if a specific one of these is misbehaving. If you have other meters with working displays it may be possible to switch 1 item at a time to test that item. For example start with cable, if both cables work with the reference test, then not the cable. Then try switching the displays. If the error follows the display, would suggest something happening with the display. If error follows meter, would suggest something happening with the meter.

Are you able to do such a test?

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 5
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-08-29 01:14 PM

1 Like
3
2561
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
‎2023-08-29 01:14 PM

Hello @dsantillan ,

Is the display also new? Are you able to communicate with the Meter? can meter read serial number of display?

Do you know firmware version of the display? (Display ad meter each have unique firmware).

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
dsantillan
Lieutenant dsantillan
Lieutenant

Posted: ‎2023-08-29 08:52 PM

0 Likes
2
2553
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
‎2023-08-29 08:52 PM

Hello Charles, 

 

Thank you for the reply. 

 

Yes, these are new were bought as PM8244. The box had the PM8000 and the RD96 in it. 

Yes, PME read the meters them just fine. I can also access via IONSetup. 

The meter does not read anything from the display. 

Please find images from the display attached. 

 

Attachments
Reply
Charles_Murison
Picard Charles_Murison Picard
Picard

Posted: ‎2023-08-30 07:59 AM

0 Likes
1
2525
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
‎2023-08-30 07:59 AM

Hello @dsantillan ,

 

When you connect to the meter with ION Setup or PME, there is a module called Factory. One of the output registers of this module is RMD serial number and RMD version. If the meter does not have this information it indicates that meter is not able to talk to the display.

 

The "system" has 3 parts, the meter, the display and the cable between display and meter. Hard to say if a specific one of these is misbehaving. If you have other meters with working displays it may be possible to switch 1 item at a time to test that item. For example start with cable, if both cables work with the reference test, then not the cable. Then try switching the displays. If the error follows the display, would suggest something happening with the display. If error follows meter, would suggest something happening with the meter.

Are you able to do such a test?

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2023-08-30 03:57 PM

0 Likes
0
2521
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
‎2023-08-30 03:57 PM

Make sure the display cable is plugged into the RMD port on the base unit (and not to the Ethernet TCP ports on the bottom side of the base unit).  The cable you are using should also support PoE (Power over Ethernet)  and should be connected directly to the base unit and not though any type of IT equipment like a router and/or switch.

Reply
dsantillan
Lieutenant dsantillan
Lieutenant

Posted: ‎2023-09-19 04:39 PM

1 Like
0
2453
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
‎2023-09-19 04:39 PM

Hello Charles, 

 

Thank you for the input. For this specific case, new patch cords were required, and then a power cycle of the units. 

 

Best regards, 

 

Douglas
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.