Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogicTM VL series- Modbus Setup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PowerLogicTM VL series- Modbus Setup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Arunprasad
Arunprasad Mentor
Mentor

Posted: ‎2023-03-12 09:53 PM

0 Likes
0
1349
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
‎2023-03-12 09:53 PM

PowerLogicTM VL series- Modbus Setup

Hello All,

We have done a small modification to the Modbus parameter setting. Modbus parameters must be configured through the expert setup menu in section 700 (see PowerLogic™ User manual paragraph 5).

• BAUD RATE (701): the valid range is 1200 - 115200 baud.
Default value = 19200.
• PARITY (702): parity to be None, Even or Odd.
Default value = Even.
Note: For PARITY = None, use 2 bits stop. For PARITY = Even or Odd, use only 1 bit stop.

In general if Parity was set as Even or Odd then set as ----> 1- bit stop

But if the Parity was set as Noe then set as----> 2 bit stop


• SLAVE ADDRESS (703): the valid range is 1 - 247.
Default value = 1.

 

The settings for baud rate and parity must be the same for all bus devices, the address must be unique for each device.

Modbus set-up VPLModbus set-up VPL

 

Arunprasad
Labels
  • Labels:
  • Power Quality
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 0
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.