Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Posted: 2018-09-04 09:48 AM . Last Modified: 2020-04-22 01:08 AM
Link copied. Please paste this link to share this article on your social media post.
Hi expert,
I have a ION7330 with kWh show display screen: 9500 kWh
But my customer want plus 500 kWh, mean we will plus 500 become 10000 kWh show display screen.
I know ION setup will be made. Please help me with arithmetic.
Thanks very much
Link copied. Please paste this link to share this article on your social media post.
If you are asking if it is possible to adjust the kW due to either line losses or inaccuracies in the PTs/CTs in use, the ION73xx line of devices does not have any built in functionality to adjust the kW readings (which are calculated directly from the PT/CT ratios and measured voltages/currents). You could however, use ION technology and design a framework that would allow you to modify kW and show some type of modified kW reading (I don't know how you would want to do this by either just adding an offset or more than likely applying some type of scaling factor).
Posted: 2018-09-04 07:58 PM
Link copied. Please paste this link to share this article on your social media post.
Hi team,
Pls help me. Thanks
Link copied. Please paste this link to share this article on your social media post.
Once you've connected to the 7330, you can use the Setup Assistant and go to the RegEdit tab (located in the Templates section) and edit the existing energy totalizers to what ever value you want.

Click on the Display button near the bottom:

Then click on the Edit button on the shown dialog which will then permit you to edit the energy values.

Press Send to save the changes to the device (make sure the checkbox is checked for any readings you wish to update).
Posted: 2018-09-06 12:35 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Roberts Lee,
Thanks for your informations. How about kW?
Link copied. Please paste this link to share this article on your social media post.
If you are asking if it is possible to adjust the kW due to either line losses or inaccuracies in the PTs/CTs in use, the ION73xx line of devices does not have any built in functionality to adjust the kW readings (which are calculated directly from the PT/CT ratios and measured voltages/currents). You could however, use ION technology and design a framework that would allow you to modify kW and show some type of modified kW reading (I don't know how you would want to do this by either just adding an offset or more than likely applying some type of scaling factor).
Posted: 2018-09-08 02:48 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Robert Lee,
Hehe. Sorry, I confuse, i forgot. Because i know kW is instantaneous value.
Thanks very much Rebert Lee
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.