Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello,
Does anyone know how many PM8000 meters can connect by Ethernet daisy chain?
PME server - <Ethernet switch> - PM8000(1) - PM8000(2) - PM8000(3) - +++ - PM8000(?)
Is there any limitation about this?
We and our customers understand that the network will shut out when the PM8000 on the way goes down.
I hope hearing from someone soon.
kind regards,
Hideki Kougo
Link copied. Please paste this link to share this article on your social media post.
Note that it is 100m between *switches* (or in this case devices). Unlike a repeater a switch handles each cable independently for collisions, etc since a switch is a store & forward mechanism for each physical layer frame from each input.
Still a really good idea to limit the amount of chaining to a smallish number because if *any* device in the chain loses power then all the downstream devices will no longer be connected to the network since the "switch" has been powered off. 🙂
Posted: 2018-09-17 01:13 PM
Link copied. Please paste this link to share this article on your social media post.
You may find this article helpful. Basically states that since each meter has a unique IP and acts as a 2 port switch you can add as many meters as your network will allow. At some point it will no longer be practical to use a single connection for so many devices but that happens at a large number. Also keep in mind that you can only have a 100 meter cable run before you need a repeater or other network device.
Link copied. Please paste this link to share this article on your social media post.
Note that it is 100m between *switches* (or in this case devices). Unlike a repeater a switch handles each cable independently for collisions, etc since a switch is a store & forward mechanism for each physical layer frame from each input.
Still a really good idea to limit the amount of chaining to a smallish number because if *any* device in the chain loses power then all the downstream devices will no longer be connected to the network since the "switch" has been powered off. 🙂
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.