Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84628members
353951posts

PM2X30 Analog Inputs (METSEPM2KANLGIO22) Configuration

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa453448_brid
Ensign Ensign
Ensign
0 Likes
2
366

PM2X30 Analog Inputs (METSEPM2KANLGIO22) Configuration

Hello Community,

I have a question regarding METSEPM2KANLGIO22, is posible to configure one of the analog inputs as 4-20 mA input and the another input as 12 .. 30 V input?

Thanks for your help, ...


Accepted Solutions
Jairo_Sacipa
Ensign Ensign
Ensign
0 Likes
1
349

Re: PM2X30 Analog Inputs (METSEPM2KANLGIO22) Configuration

we have only one option for setting analog output i.e to use current (4-20 ma) for this module.

PM2000 analog IO module can support only with 4-20mA current ranges for both input and output channels and it does not support for voltage based IO's

See Answer In Context

2 Replies 2
Jairo_Sacipa
Ensign Ensign
Ensign
0 Likes
1
350

Re: PM2X30 Analog Inputs (METSEPM2KANLGIO22) Configuration

we have only one option for setting analog output i.e to use current (4-20 ma) for this module.

PM2000 analog IO module can support only with 4-20mA current ranges for both input and output channels and it does not support for voltage based IO's

sesa453448_brid
Ensign Ensign
Ensign

Re: PM2X30 Analog Inputs (METSEPM2KANLGIO22) Configuration

Thanks a lot Jairo Sacipa