Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Hi, I need IEEE519-2014 framework and diagram for upload to ION7650.
I have seen in PME9.0 demo website that ION9k has IEEE519 icon at the diagram (see attached). This icon will show 95% percentile & 99% percentile of harmonic measurement (see attached) but I can’t see what is the details inside that icon and what is the framework of IEEE519.
I try to paste from ION9k framework provided by PME9.0 in designer by myself but all links are broken (see attached).
Therefore, I need diagram file and framework file from ION9k, those have complete link to all registers, to modify by myself.
Hope someone can help me on this.
Link copied. Please paste this link to share this article on your social media post.
Hi Chonnapan
The IEEE519-2014 framework and corresponding report in PME 9.0 is not available on the 7x50 platform. It requires ION modules only available on the ION9000 and forthcoming PM8000 and ION7400 V2.0 releases.
Best regards
Tom
Link copied. Please paste this link to share this article on your social media post.
To update about this issue, I can paste almost all modules of IEEE519 framework from ION9000 into the ION meters now. All links can be linked to all available modules those were pasted. But, after investigation, I think the paste is not successful because some ION modules don’t exist in the current firmware of the meters. Therefore, impossible to paste IEEE519 to them. I may need to wait for new firmware upgrade.
My next question is, when we can get new firmware update for ION7x50? I searched in Exchange and found that PM8k and ION7400 firmware V.2 will be released in Dec'18 or Jan'19. Can anyone inform me please?
Thank you in advance.
Chonnapan
Posted: 2018-10-10 02:54 PM
Link copied. Please paste this link to share this article on your social media post.
Hi Chonnapan,
I have a bfo case logged for you, will reply you through bfo soon.
Link copied. Please paste this link to share this article on your social media post.
Thank you very much. bFO of this case is shown in link below.
Do I need to do support request? Please advise.
Posted: 2018-10-11 09:44 AM
Link copied. Please paste this link to share this article on your social media post.
Hi Chonnapan,
There is one case open already:
https://se.my.salesforce.com/5001H00000qyZg9
I will reply to R Laxman Rao who is the L2 technical support in India.
Thanks
Leo
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.