Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

NTP protocol of the ION 8650

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • NTP protocol of the ION 8650
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
Ramasamy_N
Ramasamy_N Champion
117
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
PowerLogic
PowerLogic ION8650 series

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Rafaelsdsz
Rafaelsdsz
Explorer

Posted: ‎2021-08-30 09:11 AM

0 Likes
2
1865
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
‎2021-08-30 09:11 AM

NTP protocol of the ION 8650

Hello,

 

We are having problems with a GPS that synchronizes with ION 8650 meters via NTP protocol. This issue is occurring with two firmware versions of ION meters.

On client 1 we have the following scenario:

ION 8650 meters with firmware version 004.031.002, synchronized with GPS via NTP, configured with a 1 hour sync interval present the following failure:

 

1.png

We have 18 meters with the settings, being synchronized via NTP protocol with GPS and so far 9 meters have this type of failure without simultaneous synchronization error, and another 9 meters in the same GPS network do not have any fault. The meters request sync, which supply wrong data and time works for 1 hour as programmed in the sync interval and return to true data and time. What causes data storage at wrong data and times on the client.

2.png

On client 2 we have the following scenario:

ION 8650 meters with firmware version 004.040.001, synchronized on the same network with GPS via NTP, configured with a 1 minute sync interval at which they present the following failure:

 

3.png

We have 4 meters with the settings, being synchronized via NTP protocol with the GPS and so far 2 meters have this type of failure without simultaneous synchronization error, to which the other 2 meters on the same network do not differ any failure. The meters ask for sync, where providing wrong data and time works for a few minutes and returns to true data and time. What causes data storage at wrong data and times on the client.

What version of NTP or SNTP are the ION8650 meters using?

Have there been any NTP protocol changes in the latest firmware updates?

What might be causing it to fail?

  • Thumbnail of PowerLogic ION8650 series
    PowerLogic
    PowerLogic ION8650 series
View products (1)
Labels
  • Labels:
  • ION8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Juan_Arias
Juan_Arias Champion
Champion

Posted: ‎2021-08-30 09:23 AM

0 Likes
0
1855
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
‎2021-08-30 09:23 AM

@Charles_Murison  

Tags (1)
  • Tags:
  • english
Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2021-09-01 11:34 AM

0 Likes
0
1830
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
‎2021-09-01 11:34 AM

Hello @Rafaelsdsz 

What version of NTP or SNTP are the ION8650 meters using?
I am not 100% sure, but I believe this is V3. I know for sure V4 is not supported on the meter. Most V4 servers are backwards compatible to V3 devices.

Have there been any NTP protocol changes in the latest firmware updates?
No changes that I know of.

What might be causing it to fail?

Cannot say from this data alone. 

If possible would be good to get packet captures from this system. 
Ideally with a switch port mirroring the traffic to/from the meter to a second port where computer is capturing the Ethernet traffic. Wireshark is a common software to do this. The port mirror is important, may switches will hide traffic from ports it knows the traffic does not concern. So you might see the meter send out messages but never see what is sent back to the meter.

If you are able to capture the Ethernet traffic, would also be good to get the event log from the meter.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.