Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Is it possible to read Wh to 2 digits of precision on the PM5000 range?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Is it possible to read Wh to 2 digits of precision on the PM5000 range?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Picard Charles_Murison Picard
526
Mehran_Mehrnia
Admiral Mehran_Mehrnia Admiral
138
Ramasamy_N
Captain Ramasamy_N Captain
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
JamesAZZO
Sisko | EcoXpert Master JamesAZZO Sisko | EcoXpert Master
Sisko | EcoXpert Master

Posted: ‎2014-02-25 04:11 PM

0 Likes
5
1543
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
‎2014-02-25 04:11 PM

Is it possible to read Wh to 2 digits of precision on the PM5000 range?

We can see on the front panel that kW power readings have 5 decimal places. Is it possible to read the 5 decimal places in Modbus comms? Consequently, will you also be able to read kWh to that same 5 digits of precision?

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2014-03-03 09:36 AM

0 Likes
1
1478
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
‎2014-03-03 09:36 AM

Hi James,

     I'll try and answer your question as I've done some work with all the PM5XXX devices.  The Power parameters are passed via Modbus using standard IEEE 754 Float32 notation using 2 16-bit registers.  This will allow Power parameters such as kW to have up to 7 significant digits.  Thus for low power readings the front panel can display up to 5 decimal places (but as readings increase the # of digits after the decimal will reduce).  Software like ION:S may display using some type of fixed decimal representation or could dynamically adjust but showing more significant digits is meaningless.

For energy registers, the PM5XXX series passes values as an INT64 register in 4 x 16 bit registers (which represents only whole numbers without any decimals) but are passed at the lowest possible unit (ex. Wh instead of kWh).  Thus depending on how the software wants to display this information this could show up to 3 decimals (i.e.  if they show the label as kWH, then the number would be divided by 1000).

The front panel looks like it will still show this value with decimal places but those decimal places will never have any significance (i.e. lowest unit is 1 Wh which will show on the display as 1.0000 Wh).  Only whole numbers of Wh will be contained in the registers.

Hope this answers your questions.

See Answer In Context

Reply
Replies 5
JamesAZZO
Sisko | EcoXpert Master JamesAZZO Sisko | EcoXpert Master
Sisko | EcoXpert Master

Posted: ‎2014-03-02 04:57 AM

0 Likes
0
1478
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
‎2014-03-02 04:57 AM

Anyone?

Reply
sesa186702
sesa186702 Schneider Alumni (Retired)
Schneider Alumni (Retired)

Posted: ‎2014-03-02 06:51 AM

0 Likes
1
1478
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
‎2014-03-02 06:51 AM

What are you mentioning here? Power (kW) or Energy consumption (Wh) ?

Reply
JamesAZZO
Sisko | EcoXpert Master JamesAZZO Sisko | EcoXpert Master
Sisko | EcoXpert Master

Posted: ‎2014-03-02 03:22 PM

0 Likes
0
1478
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
‎2014-03-02 03:22 PM

Both actually, per my questions above.

We can see that kW (power) shows 5 decimal places on the front panel at low loads but Modbus only shows 3. Similar for kWh, but that might be because of the amount of whole digits able to be shown on the front panel. Software shows 3 decimals, similar to kW.

Reply
Robert_Lee
Admiral Robert_Lee Admiral
Admiral

Posted: ‎2014-03-03 09:36 AM

0 Likes
1
1479
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
‎2014-03-03 09:36 AM

Hi James,

     I'll try and answer your question as I've done some work with all the PM5XXX devices.  The Power parameters are passed via Modbus using standard IEEE 754 Float32 notation using 2 16-bit registers.  This will allow Power parameters such as kW to have up to 7 significant digits.  Thus for low power readings the front panel can display up to 5 decimal places (but as readings increase the # of digits after the decimal will reduce).  Software like ION:S may display using some type of fixed decimal representation or could dynamically adjust but showing more significant digits is meaningless.

For energy registers, the PM5XXX series passes values as an INT64 register in 4 x 16 bit registers (which represents only whole numbers without any decimals) but are passed at the lowest possible unit (ex. Wh instead of kWh).  Thus depending on how the software wants to display this information this could show up to 3 decimals (i.e.  if they show the label as kWH, then the number would be divided by 1000).

The front panel looks like it will still show this value with decimal places but those decimal places will never have any significance (i.e. lowest unit is 1 Wh which will show on the display as 1.0000 Wh).  Only whole numbers of Wh will be contained in the registers.

Hope this answers your questions.

Reply
JamesAZZO
Sisko | EcoXpert Master JamesAZZO Sisko | EcoXpert Master
Sisko | EcoXpert Master

Posted: ‎2014-03-03 11:44 PM

1 Like
0
1478
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
‎2014-03-03 11:44 PM

Thanks Robert! Exactly the answer I needed (although not what I was hoping for). I figured it was only measuring in Wh. If you can believe this, we have a customer who wants to be measuring energy down to the 0.00 of a Wh. (not kWh) - crazy and unmeaningful in 99.99999 of cases.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.