Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

In the PM5000 series meters, what is the difference between the protected and unprotected command interface?

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • In the PM5000 series meters, what is the difference between the protected and unprotected command interface?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
sesa277735
sesa277735 Leader
Leader

Posted: ‎2015-02-27 10:13 AM

0 Likes
2
1670
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
‎2015-02-27 10:13 AM

In the PM5000 series meters, what is the difference between the protected and unprotected command interface?

When sould registers 5000 - 5249 be used over 5250 - 5499?
Any examples will be very helpful!

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Usha
Usha Mentor
Mentor

Posted: ‎2015-03-23 11:11 PM

2 Likes
1
1544
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
‎2015-03-23 11:11 PM

Hi Darell,

Protected mode requires the user to obtain the semaphore before executing the command.  PM5000 supports both protected and unprotected command interfaces.  In the register list, there is a "Commands" tab.  In that tab, it lists all of the commands that can be executed by the meter under protected or unprotected mode.  It also lists the parameters that need to be specified by each command.  You can filter those commands based on the column titled: "Allowed for Unprotected Command Interface".
Registers 5000-5249 are "Protected Command Interface" registers
Registers 5250 - 5499 are "Unprotected Command Interface" registers


Using the Protected Command Interface

To issue a meter command using the protected command interface, you must have a

command semaphore.

To get a semaphore, read the semaphore Modbus register. The power meter will return a 0 or a nonzero number.

• If 0 is returned, someone else owns the semaphore. You must wait for the semaphore to be available before sending a command.

• If a nonzero number is returned, you now own the semaphore. The semaphore is provided once until it is released or has been inactive for approximately 4 minutes.

Once you have the semaphore, subsequent reads of the semaphore register will return 0 until you release the semaphore or it times out.

To send a meter command using the protected command interface:

1. Read the semaphore register and record the meter response. This is your semaphore.

2. Build the packet to be written to the command block.

3. Write the packet as a Modbus block write (enter the command number, semaphore,

and parameters at the same time).

Protected Command Block Example

6038

4. Monitor the meter response registers for validity and completion

Protected Meter Response Example

6040

5. Write the semaphore back to the semaphore register to release it for another master to use.



Using the Unprotected Command Interface

The unprotected command interface allows you to issue a broadcast command to multiple meters at once. The unprotected command interface ignores the semaphore register.

Although some applications require the unprotected command interface, it is recommended that you use the protected command interface whenever possible.

To send a meter command using the unprotected command interface:

1. Build the packet to be written to the command block.

2. Write the packet as a Modbus block write (enter the command number, any number

as the semaphore, and the parameters at the same time).

Unprotected Command Block Example

6041

3. Monitor the meter response registers for validity and completion

Unprotected Meter Response Example

6043


Regards,
Usha
Software Engineering Support

See Answer In Context

Reply
Replies 2
Usha
Usha Mentor
Mentor

Posted: ‎2015-03-23 11:11 PM

2 Likes
1
1544
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
‎2015-03-23 11:11 PM

Hi Darell,

Protected mode requires the user to obtain the semaphore before executing the command.  PM5000 supports both protected and unprotected command interfaces.  In the register list, there is a "Commands" tab.  In that tab, it lists all of the commands that can be executed by the meter under protected or unprotected mode.  It also lists the parameters that need to be specified by each command.  You can filter those commands based on the column titled: "Allowed for Unprotected Command Interface".
Registers 5000-5249 are "Protected Command Interface" registers
Registers 5250 - 5499 are "Unprotected Command Interface" registers


Using the Protected Command Interface

To issue a meter command using the protected command interface, you must have a

command semaphore.

To get a semaphore, read the semaphore Modbus register. The power meter will return a 0 or a nonzero number.

• If 0 is returned, someone else owns the semaphore. You must wait for the semaphore to be available before sending a command.

• If a nonzero number is returned, you now own the semaphore. The semaphore is provided once until it is released or has been inactive for approximately 4 minutes.

Once you have the semaphore, subsequent reads of the semaphore register will return 0 until you release the semaphore or it times out.

To send a meter command using the protected command interface:

1. Read the semaphore register and record the meter response. This is your semaphore.

2. Build the packet to be written to the command block.

3. Write the packet as a Modbus block write (enter the command number, semaphore,

and parameters at the same time).

Protected Command Block Example

6038

4. Monitor the meter response registers for validity and completion

Protected Meter Response Example

6040

5. Write the semaphore back to the semaphore register to release it for another master to use.



Using the Unprotected Command Interface

The unprotected command interface allows you to issue a broadcast command to multiple meters at once. The unprotected command interface ignores the semaphore register.

Although some applications require the unprotected command interface, it is recommended that you use the protected command interface whenever possible.

To send a meter command using the unprotected command interface:

1. Build the packet to be written to the command block.

2. Write the packet as a Modbus block write (enter the command number, any number

as the semaphore, and the parameters at the same time).

Unprotected Command Block Example

6041

3. Monitor the meter response registers for validity and completion

Unprotected Meter Response Example

6043


Regards,
Usha
Software Engineering Support
Reply
sesa277735
sesa277735 Leader
Leader

Posted: ‎2015-04-06 12:41 PM

0 Likes
0
1544
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
‎2015-04-06 12:41 PM

Hey Usha M R,

Thanks for taking the time to answer my question!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.