Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION9000 Onboard Event Log - Ethernet Alarms

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION9000 Onboard Event Log - Ethernet Alarms
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
solutions_iems-
solutions_iems-
Troubleshooter

Posted: ‎2025-07-04 04:53 AM

0 Likes
1
709
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
‎2025-07-04 04:53 AM

ION9000 Onboard Event Log - Ethernet Alarms

I have a customer who is seeing regular Ethernet alarms in the ION9000 meter event log.

 

The alarms are associated with FTP & Telnet for USER0 and appear to be triggered by the Front Panel (see attached).

 

Could an external IP be trying to access the ION9000 meter (hack)?

 

Thanks

Attachments
Labels
  • Labels:
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-07-04 08:55 AM

1 Like
0
701
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
‎2025-07-04 08:55 AM

Hello @solutions_iems- ,

A few items to note, FTP is only supported on very old firmware. Where possible I would recommend upgrading the meter to the latest firmware.

 

As for the events, User 0 is a catchall for unauthenticated communications. It is possible the customer's IT department is doing a kind of auto scans for specific ports. There are some options available to the customer.

 

A) disable the ports when not being used. FTP is used during upgrades to transfer the meter's web pages, or to collect COMTRADe files. If customer is not using COMTRADE files, FTP could be disabled unless doing firmware upgrades. Same with Telnet, the port could be disabled unless being used for a specific purpose (only common case I know of is troubleshooting).

 

B) Changing the ports to a different number from default, many scans will look for specific ports, if the meter is not using a default port the scan will not try to access the device.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-07-04 08:55 AM

1 Like
0
702
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
‎2025-07-04 08:55 AM

Hello @solutions_iems- ,

A few items to note, FTP is only supported on very old firmware. Where possible I would recommend upgrading the meter to the latest firmware.

 

As for the events, User 0 is a catchall for unauthenticated communications. It is possible the customer's IT department is doing a kind of auto scans for specific ports. There are some options available to the customer.

 

A) disable the ports when not being used. FTP is used during upgrades to transfer the meter's web pages, or to collect COMTRADe files. If customer is not using COMTRADE files, FTP could be disabled unless doing firmware upgrades. Same with Telnet, the port could be disabled unless being used for a specific purpose (only common case I know of is troubleshooting).

 

B) Changing the ports to a different number from default, many scans will look for specific ports, if the meter is not using a default port the scan will not try to access the device.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.