Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION meters - Support for IEC61850-9-2LE

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION meters - Support for IEC61850-9-2LE
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
jorge_afonso_em
jorge_afonso_em
Explorer

Posted: ‎2019-01-15 10:19 AM

0 Likes
4
2915
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
‎2019-01-15 10:19 AM

ION meters - Support for IEC61850-9-2LE

Hi Community

 

Can someone please inform if the implementation of IEC 61850-9-2LE (Process function) is supported by some ION meter. If yes please inform which type of meter to consider.

 

Thank you very much

 

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2019-01-18 09:31 AM

3 Likes
0
2899
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
‎2019-01-18 09:31 AM

IEC 61850, in very general terms, is separated into 2 parts - the Station bus and the Process bus.   The Station bus receives data from the Process bus and is used to exchange data from the substation to supervisory systems,  The performance of the Station bus is non-deterministic.   The Process bus is a high-speed, deterministic bus that provides the connection between digital sensors and merging units where sensor data is collected and shared with the Station bus.   

 

The IEC 61850-9-2 LE deals with the Process bus and defines the connection between sensors with digital outputs and merging units, or units that collect signals from digital sensors.   This is typically a very high-speed fiber optic network with deterministic response.   

 

ION meters are deployed in IEC 61850 systems at the Station bus level.  They accept input from current and voltage sensors with analog outputs.   ION meters do not support sensors with digital outputs and cannot be deployed on or receive input from the IEC 61850 Process bus.  Therefore, there are no ION meters that support IEC 61850-9-2 LE.  

See Answer In Context

Tags (1)
  • Tags:
  • "IEC 61850-9-2 LE"
Reply
Replies 4
Kevin_Morin
Kevin_Morin Mentor
Mentor

Posted: ‎2019-01-15 01:36 PM

1 Like
0
2913
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
‎2019-01-15 01:36 PM

@Daniel_Brandao hey Daniel - do you have information on the specifics of 9-2LE and if we support this with any of our meters?

Critical Power EcoXpert Program Director
Reply
Anonymous user
Not applicable

Posted: ‎2019-01-18 09:31 AM

3 Likes
0
2899
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
‎2019-01-18 09:31 AM

IEC 61850, in very general terms, is separated into 2 parts - the Station bus and the Process bus.   The Station bus receives data from the Process bus and is used to exchange data from the substation to supervisory systems,  The performance of the Station bus is non-deterministic.   The Process bus is a high-speed, deterministic bus that provides the connection between digital sensors and merging units where sensor data is collected and shared with the Station bus.   

 

The IEC 61850-9-2 LE deals with the Process bus and defines the connection between sensors with digital outputs and merging units, or units that collect signals from digital sensors.   This is typically a very high-speed fiber optic network with deterministic response.   

 

ION meters are deployed in IEC 61850 systems at the Station bus level.  They accept input from current and voltage sensors with analog outputs.   ION meters do not support sensors with digital outputs and cannot be deployed on or receive input from the IEC 61850 Process bus.  Therefore, there are no ION meters that support IEC 61850-9-2 LE.  

Tags (1)
  • Tags:
  • "IEC 61850-9-2 LE"
Reply
pml_energobit_c
pml_energobit_c
Contributor

Posted: ‎2023-01-12 06:31 AM

0 Likes
1
2374
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
‎2023-01-12 06:31 AM

Any upgrades on this subject? any compatible meters?

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2023-01-19 08:53 AM

0 Likes
0
2356
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
‎2023-01-19 08:53 AM

I cannot speak for all meters, but for ION meters still the same.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.