• About jorge_afonso_em
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
jorge_afonso_em
jorge_afonso_em
Lieutenant | EcoXpert Master
‎2025-02-24
9
Posts
1
Like Received
2
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies - L2
Live Long and Prosper
Open Hailing Frequencies
Resistance is Futile
+4
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
jorge_afonso_em
/html/rank_icons/Lieutenant.png jorge_afonso_em /html/rank_icons/EcoXpertMasterLeaf.png

ION meters - Support for IEC61850-9-2LE

Hi Community Can someone please inform if the implementation of IEC 61850-9-2LE (Process function) is supported by some ION meter. If yes please infor...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
2381 0 4

2019-01-15 10:19 AM

jorge_afonso_em
/html/rank_icons/Lieutenant.png jorge_afonso_em /html/rank_icons/EcoXpertMasterLeaf.png

In ION8650, is it possible to use the ethernet port for IEC61850 and I...

I have a project with ION8650 meters with Ethernet port where the client wants to have the meters connected to their substation automation system thro...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1223 0 2

2018-04-02 08:05 AM

jorge_afonso_em
/html/rank_icons/Lieutenant.png jorge_afonso_em /html/rank_icons/EcoXpertMasterLeaf.png

GPRS communication between PM8000 and PME 8

HiI have an application requiring GPRS communication between PME server and a couple of PM8000 meters.Does anyone have experience in similar type of a...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1670 1 2

2017-02-17 05:14 AM

jorge_afonso_em
/html/rank_icons/Lieutenant.png jorge_afonso_em /html/rank_icons/EcoXpertMasterLeaf.png

ION8650 - Socket drawing

HiWe have a project involving a douzen of ION8650 meters of socket mounting type (ref M8650C0....). As this kind of round meters is not very common in...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
1567 0 6

2017-02-01 09:39 AM

Activity Feed
  • Tagged Re: ION meters - Support for IEC61850-9-2LE on Metering & Power Quality. ‎2019-01-21 03:35 AM
  • Liked Re: ION meters - Support for IEC61850-9-2LE for Anonymous user. ‎2019-01-21 03:33 AM
  • Liked Re: ION meters - Support for IEC61850-9-2LE for Kevin_Morin. ‎2019-01-17 03:05 AM
  • Posted ION meters - Support for IEC61850-9-2LE on Metering & Power Quality. ‎2019-01-15 10:19 AM
  • Posted Re: In ION8650, is it possible to use the ethernet port for IEC61850 and ION communication (or modbus TCP) at same time? on Metering & Power Quality. ‎2018-04-03 02:35 AM
  • Posted In ION8650, is it possible to use the ethernet port for IEC61850 and ION communication (or modbus TCP) at same time? on Metering & Power Quality. ‎2018-04-02 08:05 AM
  • Posted Re: GPRS communication between PM8000 and PME 8 on Metering & Power Quality. ‎2017-02-24 07:13 AM
  • Got a Like for GPRS communication between PM8000 and PME 8. ‎2017-02-20 03:47 PM
  • Posted GPRS communication between PM8000 and PME 8 on Metering & Power Quality. ‎2017-02-17 05:14 AM
  • Posted Re: ION8650 - Socket drawing on Metering & Power Quality. ‎2017-02-03 09:34 AM
  • Posted Re: ION8650 - Socket drawing on Metering & Power Quality. ‎2017-02-03 09:32 AM
  • Posted Re: ION8650 - Socket drawing on Metering & Power Quality. ‎2017-02-03 09:26 AM
  • Posted ION8650 - Socket drawing on Metering & Power Quality. ‎2017-02-01 09:39 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.