Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION 7400 and PM8000 Modbus Map in ION Setup

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION 7400 and PM8000 Modbus Map in ION Setup
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
kurtis_eisl_ca_
kurtis_eisl_ca_
Contributor

Posted: ‎2016-06-01 04:24 AM . Last Modified: ‎2020-04-22 01:25 AM

0 Likes
2
2123
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
‎2016-06-01 04:24 AM

ION 7400 and PM8000 Modbus Map in ION Setup

Why Doesnt the Modbus Table show up in ION Setup as it does for the ION 7330 or ION 7550? Is it simply an oversight??

 

Labels
  • Labels:
  • ION Setup
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
sesa64419
sesa64419 Leader
Leader

Posted: ‎2016-06-01 07:32 AM

1 Like
1
2049
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
‎2016-06-01 07:32 AM

Hi Kurtis

This is not an oversight.

The PM8000 and ION7400 have a different implementation of Modbus than for instance the ION7650. They do not use Modbus Slave modules to make the default Modbus map. Instead, they have a default map based on the power data model which uses Data Mapping modules.

You can download the default Modbus map here:

http://www.schneider-electric.com/ww/en/download/document/PM8000_Modbus_Map?showAsIframe=true

It is not recommended to manually modify the Data Mapping modules.

If you need to modify the Modbus data your meter provides, ION Setup is the best tool. When you click Edit (on the screen you have shown) you will get options of Default, Modified, Custom and Disabled.

Default: uses the default Modbus map (see download)

Modified: add more Modbus values to the default mapped values. This uses Modbus Slave modules.

Custom: default map is disabled and the registers are available to use in a custom map created with Modbus Slave modules. (this is intended for retrofit applications where you need to make the meter's Modbus data match with a previous device)

All of this information is described in the PM8000 user manual, 7EN02-0336-01 page 49-58 and in the ION7400 user manual.

cheers,

Alana

See Answer In Context

Reply
Replies 2
sesa64419
sesa64419 Leader
Leader

Posted: ‎2016-06-01 07:32 AM

1 Like
1
2049
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
‎2016-06-01 07:32 AM

Hi Kurtis

This is not an oversight.

The PM8000 and ION7400 have a different implementation of Modbus than for instance the ION7650. They do not use Modbus Slave modules to make the default Modbus map. Instead, they have a default map based on the power data model which uses Data Mapping modules.

You can download the default Modbus map here:

http://www.schneider-electric.com/ww/en/download/document/PM8000_Modbus_Map?showAsIframe=true

It is not recommended to manually modify the Data Mapping modules.

If you need to modify the Modbus data your meter provides, ION Setup is the best tool. When you click Edit (on the screen you have shown) you will get options of Default, Modified, Custom and Disabled.

Default: uses the default Modbus map (see download)

Modified: add more Modbus values to the default mapped values. This uses Modbus Slave modules.

Custom: default map is disabled and the registers are available to use in a custom map created with Modbus Slave modules. (this is intended for retrofit applications where you need to make the meter's Modbus data match with a previous device)

All of this information is described in the PM8000 user manual, 7EN02-0336-01 page 49-58 and in the ION7400 user manual.

cheers,

Alana

Reply
kurtis_eisl_ca_
kurtis_eisl_ca_
Contributor

Posted: ‎2016-06-01 07:44 AM

0 Likes
0
2049
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
‎2016-06-01 07:44 AM

Great Answer Thanks Alana!

Kurtis
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.