Accepted Solutions
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
If they are connected, for example, like this, I would set CT Primary to 600A:
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
Summation CTs with 5A or 1A outputs work with any power meter supporting those inputs. The meter is blind to what is creating those currents.
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
At the customer the IEM3255 with Summation CTs shows only half of the real current.
What could be the reason?
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
The connections - particularly of the primaries into the summation CT may be suspect and you need to think about the proportions and size of the summing.
As I mentioned before, if it's a true 5A or 1A output, the summation of the induced current must always be less than this. Please provide the make/model - datasheet on the summation CT you are using.
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
this is only half of current, and only half power.
its a KUW1/30-200 CT from Janitza
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
Hi Sven,
This is actually Cable split core current transformer - they should probably have something like this, too:
Best regards,
Bojan
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
Hi Bojan,
yes they have a 1+1 but i think the summation does not work.
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
Exactly - Bojan's example is exactly right. It adds up the primaries, the proportions of which need to be added together.
That said - are you using a mix of 1A and 5A CTs going into the Summation CT?
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
Hi Bojan,
you are absolutely right. For 1+1 it sould be set to 400A. For 1+1+1 is should be set to 600A
Thank you very much
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
Hi,
no it is only 1+1 or 1+1+1