Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Harmonics Display Mode

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • Harmonics Display Mode
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
217
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
Anonymous user
Not applicable

Posted: ‎2017-10-03 12:33 AM

0 Likes
5
1954
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
‎2017-10-03 12:33 AM

Harmonics Display Mode

HI all,

I have a problem. When i set Harmonic Display Mode by ION setup in ION7650 (image below).

1000.PNG

But,  I see display Harmonic just V1 and I1.

10001.PNG

I want display V2, V3 Harmonic Display Mode and I2, I3 Harmonic Display Mode. How do i do that. Thanks very much.

Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 5
Anonymous user
Not applicable

Posted: ‎2017-10-03 05:59 AM

0 Likes
0
1902
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
‎2017-10-03 05:59 AM

Please help me!! Thanks very much

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-10-03 09:41 AM

1 Like
3
1903
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
‎2017-10-03 09:41 AM

The Harmonics Display Mode settings only control how values are shown for the Harmonics modules.

It's likely that Vista diagram is looking at the Harmonics Measurement modules which have different setup register which would control how to display its output registers:

You'll have to go into Advanced Mode and go to each Harmonics Measurement module to change the Display Mode individually.

[Edit]

Looking at the latest ION Setup, most Setup Assistants are designed to modify both module types so make sure you are running the latest ION Setup and try switching to the latest available template option (go to Device Properties -> Display tab and select the latest available assistant you see) and change the option via the Setup Assistant again (this should change both Harmonics and Harmonics Measurement modules settings to almost identical settings).

Reply
Anonymous user
Not applicable

Posted: ‎2017-10-04 03:30 AM

0 Likes
2
1902
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
‎2017-10-04 03:30 AM

Hi Rebert Lee,

Thanks for your support.

I tried change option for Harmonic Display Mode from Percent Fundamental to Engineering Unit.

But  I just change V1, remain V2 and V3 I can't change.

Can you see image and instruction for me change to Engineering Unit for V2 and V3.

10001.PNG

Reply
Robert_Lee
Robert_Lee Champion
Champion

Posted: ‎2017-10-04 09:35 AM

0 Likes
1
1902
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
‎2017-10-04 09:35 AM

Do *NOT* modify the individual settings but use the IEEE/IEC settings wizard (highlight any of the bottom 10 options, and click on the IEEE/IEC button).  Select Custom on the first dialog, proceed through each dialog selecting each option from the available lists.  After pressing Finish, all necessary modules should be updated automatically do what ever setting you select (including doing both Harmonics and Harmonics Measurement modules).

Alternatively, you will need to go into Advanced ION Setup View and go to both the Harmonics Modules and Harmonics Measurement modules and modify each module to have the setting you want for Display Mode.

Lastly you will need to modify the Vista diagram since some of the labels are fixed.

Reply
Anonymous user
Not applicable

Posted: ‎2017-10-04 10:02 AM

0 Likes
0
1903
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
‎2017-10-04 10:02 AM

HI Robert,

Thanks very much. I did it. hehe
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.