Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84572members
353845posts

BCPMSCE as a Modbus TCP Gateway

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

sesa249074_brid
Ensign Ensign
Ensign
0 Likes
1
252

BCPMSCE as a Modbus TCP Gateway

Hi,

 

Do you know if a BCPMSCE may be used as a Modbus TCP Gateway. From the manual/spec it supports both Modbus TCP and Modbus RTU but it's not clear if this can be used as a gateway for slave devices.

 

Specifically I have a BCPMSCE60S (MB TCP/RTU) connected via ethernet and I have a PM5310 (MB RTU) in the same panel. Can I connect the PM5310 to the RS-485 terminals on the BCPMSCE60S and use this as the gateway.

 

kind regards,

 

Ray

1 Reply 1
Tom_Stevenson
Picard Picard
Picard
0 Likes
0
243

Re: BCPMSCE as a Modbus TCP Gateway