Posted: 2024-03-18 05:38 AM
filter fast digital input
What it the easiest way to filter a fast digital input ? I am reading a turbine type flow meter on FDI1 and I would like to have a result that does not change permanently but is "averaged" every 10 seconds for example.
I think it is likely that there are some FB´s already developed for this use.
- Labels:
-
HVAC
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
Posted: 2024-03-18 02:10 PM
Hi,
Did you know OSCAT ? Based on this you could try one of the attached filter FBs.
The description of any of these Blocks is in the link above.
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
Posted: 2024-03-18 02:10 PM
Hi,
Did you know OSCAT ? Based on this you could try one of the attached filter FBs.
The description of any of these Blocks is in the link above.
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
Posted: 2024-03-21 10:50 AM
Yes. I remember you told me some time ago you were willing to import OSCAT´s functions to TM172 format, I guess this is part of your effort. Thank you for sharing it.
I tried to compile a very simple example:
I got this error:
FILTER_MAV_DW(13) - error S1305: INC1 => Unknown function
So I downloaded it from a Siemens forum, is this code ok ?
IF X >= N - 1 THEN
INC1 := 0;
ELSE
INC1 := X + 1;
END_IF;
(* this elegant version is 50% slower
INC1 := X := (x + 1) MOD N;
*)
Is explicit dword to udint conversion as per my example needed or can I just :
They both compile fine.
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
Posted: 2024-03-26 03:57 AM
This is a Mastercard´s gift, it´s priceless 😊. Thank you.
If you would like me to help please do let me know. I will be happy to do it.
Regards
Link copied. Please paste this link to share this article on your social media post.