Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84295members
353434posts

Simulating LMC058 controller with ethernet port in soMachine software

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

Solved
jerryvdk
Crewman
Crewman
0 Likes
1
771

Simulating LMC058 controller with ethernet port in soMachine software

Hi all,

 

Is it possible to simulate LMC058 PLC with ethernet in soMachine software. I want to test the logic written in PLC which uses tcpudp library.

 

 

Tags (1)

Accepted Solutions
SimA
Ensign Ensign
Ensign

Re: Simulating LMC058 controller with ethernet port in soMachine software

Unfortunately, some functions/libraries that are linked to hardware communication ports cannot be simulated without a controller.  You can simulate the SoMachine / Machine Expert protocol to simularte HMI/Scada communication but you can't simulate raw tcp/udp from the TcpUdpCommunication library. 

 

You will need a physical controller to test you tcp udp communication.  If you don't have a LMC058, you could test that part on a M258, M241 or M251.

See Answer In Context

Tags (1)
1 Reply 1
SimA
Ensign Ensign
Ensign

Re: Simulating LMC058 controller with ethernet port in soMachine software

Unfortunately, some functions/libraries that are linked to hardware communication ports cannot be simulated without a controller.  You can simulate the SoMachine / Machine Expert protocol to simularte HMI/Scada communication but you can't simulate raw tcp/udp from the TcpUdpCommunication library. 

 

You will need a physical controller to test you tcp udp communication.  If you don't have a LMC058, you could test that part on a M258, M241 or M251.

Tags (1)