Issue
Users need to determine the version or build number of the Sigma software installed on their system.
Product Line
Satchwell Sigma
Environment
Satchwell Sigma
Cause
Sigma software installations are identified by build numbers, not just release numbers. This can cause confusion when troubleshooting or verifying compatibility.
Resolution
To identify the Sigma release and build number:
- Open the Sigma Client on the Sigma Server.
- Navigate to Help > About System Manager.
- A window will display both the release number and build number.
Reference Table
Use the table below to match build numbers with their corresponding release versions and file dates.
| Sigma Release No. | Build No. | Software/Firmware | File Date |
SigmaX
|
| Release 1 | 1.52 | Software/Firmware | 22.06.2001 | SigmaX 4.5 |
| Release 2 | 2.13 | Software/Firmware | 14.02.2002 | SigmaX 5.2 |
| Release 2 | 3.12 | Supplement | 14.02.2002 | SigmaX 5.2 |
| Release 3 | 3.12 | Software | 31.07.2002 | SigmaX 5.2 |
| Release 3.1 | 3.17 | Software | 17.09.2002 | SigmaX 5.2 |
| Release 3.3 | 3.3 | Software | 30.07.2003 | SigmaX 5.2 |
| Release 3.4 | 3.31.1 | Software | 03.10.2003 | SigmaX 5.2 |
| Release 3.6 | 3.32.10 | Software | 19.11.2003 | SigmaX 5.2 |
| Release 3.7 | 3.33.9 | Software | 22.12.2003 | SigmaX 5.2 |
| Release 3.7 SP2 | 3.33.11 | Software | 27.01.2004 | SigmaX 5.2 |
| Release 3.7 SP3 | 3.33.13 | Software | 19.02.2004 | SigmaX 5.2 |
| Release 3.10 | 3.34.11 | Software | 21.04.2004 | SigmaX 5.2 |
| Release 3.11 | 3.34.11 | Supplement | 31.08.2004 | SigmaX 5.2 |
| Release 4.00 | 3.36.11 | Software | 16.12.2005 | SigmaX 6.0.1 |
| Release 4.00 SP2 | 3.36.16 | Software | 02 03 2006 | SigmaX 6.0.1 |
| Release 4.00 SP4 | 3.36.20 | Software | 23.05.2006 | SigmaX 6.0.1 |
| Release 4.01 | 3.37.08 | Software | 07.09.2006 | SigmaX 6.0.1 |
| Release 4.01 SP1 | 3.37.09 | Software | 26 09 2006 | SigmaX 6.0.1 |
| Release 4.01 SP3 | 3.37.12 | Software | 20 10 2006 | SigmaX 6.0.1 |
| Release 4.01 SP4 | 3.37.13 | Software | 13 08 2006 | SigmaX 6.0.1 |
| Release 4.01 SP4a | 3.37.16 | Software | 17 11 2006 | SigmaX 6.0.1 |
| Release 4.01 SP5 | 3.37.18 | Software | 05 01 2007 | SigmaX 6.0.1 |
| Release 4.02 | 3.39.09 | Software | 26 01 2007 | SigmaX 6.0.1 |
| Release 4.03 | 3.40.06 | Software | 06 06 2007 | SigmaX 6.0.1 |
| Release 4.03 Sp1 | 3.40.09 | Software | 09 08 2007 | SigmaX 6.0.1 |
| Release 4.04 | 3.41.14 | Software | 27.02.2008 | SigmaX 6.0.1 |
| Release 4.04 SP1 | 3.41.15 | Software | 09.05.2008 | SigmaX 6.0.1 |
| Release 4.04 SP2 | 3.41.16 | Software | 15 09 2008 | SigmaX 6.0.1 |
| Release 4.04 SP3 | 3.41.18 | Software | 08 01 2009 | SigmaX 6.0.1 |
| Release 4.04 SP4 | 3.41.19 | Software | 08 01 2009 | SigmaX 6.0.1 |
| Release 4.05 | 3.42.34 | Software | 06 11 2009 | SigmaX 6.0.1 |
| Release 4.05 SP1 | 3.42.43 | Software | 22 03 2010 | SigmaX 6.0.2 |
| Release 4.05 SP2 | 3.42.48 | Software | 26.08.2010 | SigmaX 6.0.2 |
| Release 4.05 SEB | 3.43.18 | Software | 08 12 2010 | SigmaX 6.0.2 |
| Release 4.06 | 3.44.14 | Software | 01 12 2011 | SigmaX 6.0.2 |
| Release 4.06 SP1 | 3.44.16 | Software | 01 12 2011 | SigmaX 6.0.2 |
| Release 4.06 SP1 | 3.44.18 | Hotfix | 01 02 2012 | SigmaX 6.0.2 |
| Release 4.07 | 3 45 48 | Software | 20 08 2012 | SigmaX 7.0.6 |
| Release 4.07 SP1 | 3 45 51 | Service Pack | 09 12 2012 | SigmaX 7.0.6 |
| Release 4.07 SP2 | 3 45 58 | Service Pack | 20 12 2013 | SigmaX 7.0.6 |
| Release 4.08 | 3.46.57 | Software | 10 04 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.62 | Hotfix | 21.05.2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.70 | Hotfix | 23 07 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.72 | Hotfix | 04 08 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.73 | Hotfix | 12 08 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.79 | Hotfix | 08 10 2014 | SigmaX 7.0.7 |
| Release 4.08 (**1) | 3.46.80 | Software | 10 04 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.81 | Hotfix | 17 02 2015 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.85 | Hotfix | 19 03 2015 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.86 | Hotfix | 19 03 2015 | SigmaX 7.0.7 |
| Release 4.08 (**2) | 3.46.89 | Software | 10 04 2014 | SigmaX 7.0.7 |
| Release 4.08 | 3.46.98 | Hotfix | 14 12 2016 | SigmaX 7.0.7 |
| Release 4.08 (**3) | 3.46.104 | Software | 28 02 2017 | SigmaX 7.0.9 |
| Release 4.08 | 3.46.105 | Hotfix | 10 03 2017 | SigmaX 7.0.9 |
| Release 4.08 (**4) | 3.46.106 | Software | 28 03 2017 | SigmaX 7.0.9 |
| Release 4.08 | 3.46.107 | Hotfix | 08 08 2017 | SigmaX 7.0.9 |
| Release 4.08 | 3.46.108 | Hotfix | 01 05 2018 | SigmaX 7.0.9 |
| Release 4.08 (**5) | 3.46.110 | Software | 13 05 2019 | SigmaX 7.0.9 |
| Release 4.08 (**6) | 3.46.111 | Hotfix | 15 11 2019 | SigmaX 7.0.9 |
| Release 4.08 (**7) | 3.46.131 | Software | 29 01 2020 | SigmaX 7.0.9 |
| Notes: | ||||
| **1 Sigma build 4.46.57 with StruxureWare Building Operation v1.5 or 1.6 transition support program installed. | ||||
| **2 Sigma build 4.46.57 with StruxureWare Building Operation v1.8 transition support program installed. | ||||
| **3 Sigma build 4.46.57 with StruxureWare Building Operation v1.9 transition support program installed. | ||||
| **4 Sigma build 3.46.57 with StruxureWare Building Operation v2.01 transition support program installed. | ||||
| **5 Sigma build 3.46.57 with StruxureWare Building Operation v3.0.1, v3.0.2 and v3.0.3 transition support program installed.. | ||||
| **6 Sigma build 3.46.57 with StruxureWare Building Operation v3.0.4, v3.1 and v3.2 transition support program installed. | ||||
| **7 Sigma build 3.46.57 with StruxureWare Building Operation v3.2 or later transition support program installed. | ||||
Notes:
1. SigmaX version 7.0.9 is now available and can be used on any Sigma version that supported SigmaX version 7.0.6.
2. This information can be downloaded as a PDF file: Sigma Build Numbers 2023
3. When SigmaX 6.0.2 is installed, the build information provided by Sigma (Help > About) can be wrong (later than the actual version). This arises because SigmaX installs a file with Build 3.42.47 in the c:\sigma\bin folder. This is only a problem prior to Sigma Release 4.05 SEB.
⚠️ Important Notice
Sigma is not supported in EBO 2022 and later.
To continue supporting Sigma devices, you can implement a multi-version system:
- Keep Enterprise Servers with Sigma devices on Building Operation 3.2.
- Add a Building Operation 2022 or later Enterprise Central
- Upgrade the rest of the system to Building Operation 2022 or later.
You will not be able to upgrade EcoStruxure Building Operation servers that contain unsupported protocols, objects, or devices. Attempting to do so will result in failed upgrades or loss of functionality.