Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Posted: 2023-06-0809:29 PM
I use various laser profilometers & cameras as PoE. I also on occasion will use a PoE splitter to get power to a non PoE device which is nice if you want to minimize what's running through a drag chain or robot dress pack. It's a nice to have right now definitely not a need to have. One last thing make sure maintenance understands PoE and has spares for injectors, switches, and splitters
Link copied. Please paste this link to share this article on your social media post.
Posted: 2023-06-1201:52 AM
PoE is starting to appear on the valve actuators (re:SP90), power is needed to be injected every 7 to 10 devices. Specific cables are used to connect and daisy chain devices, IP water ingress protection is partly the reason for the specific cables.