Posted: 2021-08-12 07:13 AM
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
Posted: 2021-08-12 07:13 AM
STB and DDT equipment
Hello
The documentation says that the modules are identified by their position in the island which is therefore used to generate an "ID" + position.
I have the configuration below
STB
When it is integrated via the DTM in unity pro, I recover from the following equipment DDT where it can be seen that the "IDs" do not correspond at all to the position of the module.
DDT STB
I don't understand why ?
I use Unity pro V12 and advantys
- Labels:
-
Smart Design & Engineering
- Tags:
- english
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
Posted: 2021-10-21 08:18 AM
Hello @Rodrigo_Garcia , sorry not heard about this
I suggest to submit this to Schneider Electric Expert support you will get the answer.
I m sure you will get answer
- Tags:
- english
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
Posted: 2021-10-21 09:04 AM
Did you remove modules from the initial configuration or have you made any changes to the configuration? if you do that then the IDx will not line up. if you create a USER Defined label within Advantys rather than allowing Unity to create the variable for you then the Variable will always line up with the slot you are using.
- Tags:
- english
Link copied. Please paste this link to share this article on your social media post.