Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84455members
353661posts

Control Expert Simulator only allows one connection

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
rudi_accuvar_co
Crewman
Crewman
0 Likes
2
700

Control Expert Simulator only allows one connection

Hi,

 

I am running Control Expert V15 SP1. If I start the simulator I can connect to it from Control Expert and download the program to it and monitor it and Control Expert stays connected. As soon as I try to connect to the simulator from another software package eg. Vijeo Designer, then Control Expert loses its connection to the simulator. Vijeo Designer is now connected with no problems and I can simulate the running PLC, but Control Expert will not connect again while the Vijeo Designer connection is active. I have to stop Vijeo Designer first before Control Expert will connect again to the simulator. It seems as if the simulator only allows one connection at a time.

Tags (1)

Accepted Solutions
Michael_Chan
Lt. Commander Lt. Commander
Lt. Commander

Re: Control Expert Simulator only allows one connection

Hi,

 

This was a known issues when you use the first release version of Control Expert V15.0 SP1. The PLC Simulator accept only one TCP connection.

Attached herewith is the Hotfix for the Control Expert V15.0 SP1.

Try this out and it should solve your issues.

 

With Regards,

Michael Chan Kum Yuen

See Answer In Context

Attachments
Tags (1)
2 Replies 2
Michael_Chan
Lt. Commander Lt. Commander
Lt. Commander

Re: Control Expert Simulator only allows one connection

Hi,

 

This was a known issues when you use the first release version of Control Expert V15.0 SP1. The PLC Simulator accept only one TCP connection.

Attached herewith is the Hotfix for the Control Expert V15.0 SP1.

Try this out and it should solve your issues.

 

With Regards,

Michael Chan Kum Yuen
Attachments
Tags (1)
rudi_accuvar_co
Crewman
Crewman
0 Likes
0
666

Re: Control Expert Simulator only allows one connection

Hi Michael,

 

The hotfix fixed the problem.

 

Thanks for the help.

 

 

Tags (1)