Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

M172 HMI message pop-up

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • M172 HMI message pop-up
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Related Products
product field
Schneider Electric
EcoStruxure™ Machine Expert - HVAC

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to HVAC and Pumping Forum
Start a Topic
otrotabi
otrotabi
Contributor

Posted: ‎2023-02-14 08:32 AM

0 Likes
3
2797
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
Posted: ‎2023-02-14 08:32 AM

M172 HMI message pop-up

I am trying to make alarms visible on a "pop-up" screen in M172 HMI. I do it by using a "Message" instead of a regular page.  An example code is available here .

 

I define a couple of status variables to do this and use them in a GlobalOnTimer procedure. ActiveAlarm is ON whenever at least one alarm is active, and AlarmIgnore is used to tell the PLC to stop sending alarms for some time:

 

//ActiveAlarm : at least one alarm is active


uiret:=Video_GetParam(0,Addr_ActiveAlarm,0,?ActiveAlarm,tyBool); // See if alarms are active

//AlarmIgnore : tell the PLC not to cycle alarms
uiret:=Video_GetParam(0,Addr_AlarmIgnore,0,?IgnoreAlarm,tyBool); // See if alarms are acknowledged

//Alarm Pop Up screen

IF ActiveAlarm THEN
	IF NOT AcknowledgeAlarm THEN 
		msg_id_opened:=1; //Make sure what page number is loaded
		uiret:=Video_SendEvent(kWM_MSG,msg_id_opened);  
	END_IF;
ELSE	
	IF HMI_usiPosition = 1 THEN
		msg_id_opened:=0; 
		uiret:=Video_SendEvent(kWM_KEY,kKEY_VK_F3); //Close pop up
		//Define global virtual key VK_F3 as close
	END_IF;	
	AcknowledgeAlarm := FALSE;
END_IF;	

 

There´s a couple of minor corrections needed but the code works both in simulation and on a physical target (TM172PDG18R), as long as I connect to the target and "Download all" the project.

 

However, if I need to correct the HMI code or screens, I can connect to the PLC but when I finish the process of downloading the new HMI code, PLC hangs and I get either WDT3 or HMI can not be loaded error when the PLC starts. 

 

So, the problem lies on the GlobalOnTimer procedure. If I remove the Video_SendEvent function and open the screen with a button instead, there are no issues.

 

Any comments on how to improve this will be welcome.

 

 

 

Labels
  • Labels:
  • HVAC
  • Tags:
  • Ecostruxure HVAC
  • english
  • TM172
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
Bastian_Schmitz
Bastian_Schmitz Champion
Champion

Posted: ‎2023-02-14 08:37 AM . Last Modified: ‎2023-02-14 08:38 AM

0 Likes
0
2795
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
Posted: ‎2023-02-14 08:37 AM . Last Modified: ‎2023-02-14 08:38 AM

sysHMI_Message.PNG

 

Hi,

So far I remember exactly for this purpose is the Target function sysHMI_Message in Programming integrated. 

 

 

Attachments
Reply

Link copied. Please paste this link to share this article on your social media post.

otrotabi
otrotabi
Contributor

Posted: ‎2023-02-14 09:26 AM

0 Likes
0
2790
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
Posted: ‎2023-02-14 09:26 AM

Thanks Bastian for the tip.

 

Do you remember if there´s anyway to close the popup from programming ? I tried setting the input to a not valid value but it does not close it. Or do I need to write an OnTimer procedure in the message screen ?

 

hmipop.jpg

Reply

Link copied. Please paste this link to share this article on your social media post.

FedericoM
FedericoM Mentor
Mentor

Posted: ‎2023-02-17 02:13 PM

0 Likes
0
2745
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
Posted: ‎2023-02-17 02:13 PM

Hi,

 

the limit of sysHmi_Message() is that it works only on local display and not on the remote TM17xDGRP.

The reason of the watchdog I think is that the code tries to open infinite time the popup.

 

I haven't tested it, but try to modify the code more or less in this way:

GLOBAL TIMER SCRIPT: 

//ActiveAlarm : at least one alarm is active

 

uiret:=Video_GetParam(0,Addr_ActiveAlarm,0,?ActiveAlarm,tyBool); // See if alarms are active

 

//AlarmIgnore : tell the PLC not to cycle alarms

uiret:=Video_GetParam(0,Addr_AlarmIgnore,0,?IgnoreAlarm,tyBool); // See if alarms are acknowledged

 

//Alarm Pop Up screen

 

IF ActiveAlarm THEN

        IF NOT AcknowledgeAlarm AND NOT(xMsg1Open) THEN

                 msg_id_opened:=1; //Make sure what page number is loaded

                 xMsg1Open:=TRUE;

                 uiret:=Video_SendEvent(kWM_MSG,msg_id_opened); 

        END_IF;

ELSE   

        AcknowledgeAlarm := FALSE;

END_IF;

 

ONTIMER SCRIPT of the Message: 

IF NOT(ActiveAlarm) THEN

        xMsg1Open:=FALSE;

         uiret:=Video_SendEvent(kWM_KEY,kKEY_VK_F3); //Close pop up

END_IF;      

 

Close button of the Message must call the same script linked to OnTimer
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.