Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
Search in
 tfranklin
		
		
		
		
		
		
		
		
	
			 on 
    
	
		
		
		2022-06-13
	
		
		07:28 AM
		
			tfranklin
		
		
		
		
		
		
		
		
	
			 on 
    
	
		
		
		2022-06-13
	
		
		07:28 AM
	
	
	
	
	
	
	
	
	
	
	
	
	
	
		
	
				
		
	
		We've recently run into a few installs where users who previously had WebX utilized the copy to clipboard function that existed on the bottom right corner of the embedded list. Upon going to VVX they've lost this ability since the native list in ViewX for some reason does not have this capability.
We've scripted a copy to clipboard function in the past that uses the cmd clip function, but that doesn't seem to function in VVX. I've since resorted to one of two workarounds --
1) Have a button open the query in a native ViewX list that they can then ctrl+c on.
2) Change the functionality altogether to export the data to a CSV which is then downloaded to the client.
Both of these work, but users have commented that this loss of functionality caused a bit of grief.
There's another thread in these forums that myself or maybe Dustin Symes had made about a modernized embedded list object. I think this would be the most ideal time to consider something like that, where copy to clipboard is native to it along with some other features like inline grouping and filtering.
Link copied. Please paste this link to share this article on your social media post.

Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.