Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Allow Alarm Severities to be set back to blank in ViewX

Geo SCADA and Remote Operations Devices Ideas

Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
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
  • Remote Operations
  • Geo SCADA and Remote Operations Devices Ideas
  • Allow Alarm Severities to be set back to blank in ViewX
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
  • Alphabetical
  • SCADA 2
  • ViewX 2
  • Mimics 2
  • SCADAPack 2
  • Scripting 1
  • Virtual ViewX 1
  • Geo SCADA Expert 1
  • Efficiency 1
  • Configuration management 1
  • Modbus to WiStar 1
Idea Statuses
  • Submitted 14
  • Under consideration 139
  • Accepted 1
  • Declined 5
  • Partially delivered 0
  • Delivered 3
  • Abandoned 0
Related Products
Thumbnail of EcoStruxure™ Geo SCADA Expert
Schneider Electric
EcoStruxure™ Geo SCADA Expert
118
Thumbnail of SCADAPack 57x
Schneider Electric
SCADAPack 57x
2
Thumbnail of Accutech
Schneider Electric
Accutech
1
Load more
Completed Ideas
  • Tag Bit addressing for the EtherNet/IP driver

  • Geo SCADA Expert as OPC-UA server

  • OPC-UA Driver

  • API driver

  • Accutech Modbus Master gateway to read Modbus devices and incorporate into WiStar net

View All
Top Liked Authors
User Likes Count
GeoffChisholm
GeoffChisholm
2
rlao
rlao
1
View All

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
1 Like

Allow Alarm Severities to be set back to blank in ViewX

Status: Under consideration Submitted by srigby on ‎2022-02-19 04:37 PM
4 Comments (4 New)

When using ViewX to configure an alarm severity on a point, once the alarm severity is set and the point is saved, it is no longer possible to set the severity back to the default state (a blank severity).

 

I'll illustrate with an example. Open ViewX and configure an analog input point. Choose an alarm and change the Severity Type from None to Event or Alarm, you are then able to change the Severity to Maintenance, Low, High or Critical. If you then save this configuration but later change your mind and set the Severity Type back to None, the Severity remains set albeit greyed out (ie: Maintenance, Low, High or Critical). The Severity in this case is irrelevant and it would be nice if it were set back to empty (Severity of 0).

 

I know I can use the scripting (an UPDATE statement for instance) or use the Bulk Edit Tool to set the severity back to zero but it should be possible to do this from ViewX. Are there any plans on changing ViewX to allow the severity to be reset to empty in future releases of GeoSCADA?

Tags (5)
  • Find more ideas tagged with:
  • english
  • scada
  • SCADA app
  • SCADA software
  • SCADA tutorial
Comment

Link copied. Please paste this link to share this article on your social media post.

  • Back to Idea Exchange
  • Previous
  • Next
4 Comments
BevanWeiss
BevanWeiss
Champion
‎2022-02-20 02:27 PM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-02-20 02:27 PM

If the Severity Type is not valid (i.e. not Event / Alarm / Fleeting), then the Severity value has no meaning for this Severity Type setting, and hence retains it's current value (because there is no reason to change it).

 

I very much prefer the current behaviour.

 

It allows us to change between None / Event / Alarm / Fleeting without the actual Severity value becoming invalidated.

So it's possible to go from Alarm -> None.  And then at a later time from None -> Alarm and the alarm severity value is maintained through this.

srigby
srigby
Contributor
‎2022-02-21 01:50 PM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-02-21 01:50 PM

Thanks for this reply.

 

I acknowledge that for your scenario (changing Alarm -> None and at a later time changing back from None to Alarm) would be useful as a way of temporarily disabling an alarm and enabling it again at a later stage without having to remember what the alarm severity was.  So, maybe the current behaviour for this scenario doesn’t need to change.

 

What DOES need to change is the ability to remove (or set back to default) a configuration that is no longer correct.  The current ViewX system allows you to configure an alarm type and severity and once saved, no longer allows you to change it back to a blank state.  Please understand that this behaviour is incredibly frustrating.  Once left in this state, an operator would see an alarm severity that is totally meaningless if the severity type is set to “None”.  I am working on a database at present where there are literally thousands of points that exhibit this behaviour.

 

Please consider changing the interface in ViewX so that once an alarm or event is configured, the severity type can later be reset back to default.  This could be done by adding an additional entry into the Severity drop-down box of “None”.

sbeadle
sbeadle Champion
Champion
‎2022-02-22 03:43 AM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-02-22 03:43 AM
Status changed to: Under consideration

Thank you for all your comments, the feedback is appreciated. We will review your contributions.

 

Kind regards

Steve

srigby
srigby
Contributor
‎2022-02-22 08:14 PM
  • Mark as Read
  • Mark as New
  • Bookmark
  • Permalink
  • Print
  • Email to a Friend
  • Report Inappropriate Content
‎2022-02-22 08:14 PM

Thanks Steve.

Comment
Preview Exit Preview

never-displayed

Hint:
@ links to members, content
 
  • Back to Idea Exchange
  • Previous
  • Next
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.