Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Sockets

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • Sockets
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 06:14 PM
0 Likes
0
1777
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
‎2021-06-09 06:14 PM

Sockets

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 10, 2021 03:14 AM

📖 Home  Back  

Overview

Sockets provide communications between DBserver, drivers, clients and the outside world. As with all resources on computers the possible sockets available for use are limited and if they get used up it can cause problems with ClearSCADA.

By default, on Windows, the ephemeral ports are in the range 1024 to 5000. Ephemeral ports are allocated to processes need to be able to communicate but don't require a specific port number. ClearSCADA uses ephemeral ports for the following communications:

 

  • ViewX to server connections

 

  • Server to ViewX advise connections

 

  • WebX to server connections

 

  • Server-driver connections

 

  • Telnet listen ports for diagnostics

If you run out of sockets the above connections may have problems establishing fully (or at all) and so you will have problems on the system, such as drivers not starting or ViewX not connecting. Remote diagnostic facilities (Remote Desktop, VNC, remote file access, etc) will also likely be affected.

Finding Out Socket Usage

The simplest way to find out the sockets currently in use is to use the inbuilt Windows netstat command.

'netstat -ano' or 'netstat -bn'


The above command will list all active sockets. You will be able to see sockets that are waiting for a connection, have established, are waiting to expire, etc. If you see a large number of sockets and the range 1024-5000 all showing in use this indicates a potential socket issue. Note that netstat shows all sockets, not just those on the ephemeral ports.

Sadly netstat doesn't show which process is using which socket, all it tells you is how many sockets are in use. To find out which socket is being used by which process (and so which process could be having issues) you can use the Sysinternals] tool TCPView. This is a graphical tool that will show real-time information about sockets and their owning process.

tcpview.pngtcpview.pngtcpview.png
The above screenshot shows an example TCPView session (PL183 is the local host name). It has examples of dbserver.exe listening on port 5481 and 8080, an outgoing client advise connection to port 5500 and an incoming client connection from port 4971.

The above screenshot also shows the example dbserver-driver connection, for example between dbserver and DriverModbusSlave on ports 4979 and 4974 respectively.

TCPView also comes with tcpvcon.exe, a command line based version which can be used in place of netstat in automated batch files.

tcpvcon -anc

Causes of Increased Sockets

The following items list possible causes as to why you are using more sockets than "normal"

 

  • Each ViewX client will use a few sockets.

 

  • Other clients will use sockets, although less of them.

 

  • TCP/IP outstations will all make individual socket connections.

 

  • Resource leak, such as a bug in code not closing sockets when not in use anymore or network card driver issues.

Increasing the Available Ports

The default range of 1024-5000 is fine for normal usage however with ClearSCADA it sometimes isn't enough. There are two options, both of which can be implemented as deemed necessary.

Increasing the Range

You can increase the maximum port value from the default 5000. This is configured in

HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\Tcpip\Parameters\MaxUserPort (REG_DWORD)


Setting this value to be higher and rebooting increases the port range. A suggested change is to 15,000 (0x3A98), maximum is 65,534 (0xFFFE)

See http://support.microsoft.com/kb/196271 for more information from Microsoft.

Decreasing the Timeout

When a socket is closed it hangs around in memory in case the process wants to use it again (see TIMED_WAIT in above screenshot). This is for efficiency reasons but can mean more sockets are out of selection if a lot of sockets close and open regularly. The timeout it waits can be dropped from the default of 240 to something less as required.

HKEY_LOCAL_MACHINE\SYSTEM\CurrentControlSet\Services\Tcpip\Parameters\TcpTimedWaitDelay (REG_DWORD)

 

Valid range is 30-300 (0x1E-0x12C). A suggested value to try is 60 or 90. Again a reboot is required for the changes to take effect.

See http://support.microsoft.com/kb/149532 for more information from Microsoft.

See http://www.samag.com/documents/s=1176/sam9907d/9907d.htm for some useful information on TCP connection states and problems.

Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.