Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 09:48 PM
| Property | Internal Point | Database Variable | Parameter | Comment |
|---|---|---|---|---|
| Database icon | Dark Grey | Yellow | Light Grey | |
| Which data steam are the values stored within? | Data stream | Data stream | Config stream | The choice of which steam is important should you export/import the object via SDE. SDE files only contain the config stream so on import the internal point and database variable will have no value |
| Permission required to change value | Control | Control | Configure | Generally operators will have the Control permissions but not Configure, this can be used to control who can change the value |
| Alarms | Analogue and digital: Yes String and Time: No | No | No | |
| Historic | Analogue and digital: Yes String and Time: No | No | No | |
| Value change logging | Standard event logging | Standard event logging | Config Changes table, if enabled | |
| Includes in count for licensing? | Yes | No | No | |
| Included data types | Analogue digital string time | Lots, including (array for some): Boolean, byte colour (RGB) double floats strings time variants | Postal address double grid reference object link parameter table string | |
| Triggers logic on-input changed | Analogue and digital: Yes String and Time: No | No | No |
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.