Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

ClearSCADA 2009 R2.2 Operating System Support

Geo SCADA Knowledge Base

Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
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
  • Geo SCADA Knowledge Base
  • ClearSCADA 2009 R2.2 Operating System Support
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Top Labels
Top Labels
  • Alphabetical
  • database 32
  • Web Server and Client 31
  • WebX 19
  • Request Form 18
  • Lists, Events & Alarms 16
  • ViewX 15
  • Setup 12
  • Application Programming 12
  • Telemetry 8
  • Events & Alarms 7
  • Lists 7
  • Mimic Graphics 7
  • Downloads 6
  • Geo SCADA Expert 5
  • SCADA 5
  • IoT 5
  • Support 5
  • Drivers and Communications 4
  • Security 4
  • 2025 3
  • IEC 61131-3 Logic 3
  • DNP 3 3
  • Virtual ViewX 2
  • Trends and Historian 2
  • Architectures 1
  • Templates and Instances 1
  • Releases 1
  • Maps and GIS 1
  • Mobile 1
  • Geo Scada 1
  • Tools & Resources 1
  • Privacy Policy 1
  • OPC-UA 1
  • ClearSCADA 1
  • Python 1
  • Previous
  • 1 of 4
  • Next
Latest Blog Posts
  • Python API - Reading the Instance and Template Structure
  • Python API - How to get Earthquake data into a Geo SCADA Map
  • Python API - Creating and Configuring Data Tables
  • Python API - Setting aggregates
  • Python API - Clearing an aggregate link
Related Products
product field
Schneider Electric
EcoStruxure™ Geo SCADA Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Anonymous user
Not applicable
‎2021-06-09 09:39 AM
0 Likes
0
708
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
‎2021-06-09 09:39 AM

ClearSCADA 2009 R2.2 Operating System Support

Originally published on Geo SCADA Knowledge Base by Anonymous user | June 09, 2021 06:39 PM

📖 Home  Back  
Systems running on server hardware need to use server operating systems such as Windows Server 2008, Windows Server 2003, or Windows Server 2000. Server operating systems are designed for servicing entire systems rather than individual computers or small networks and so are better suited for larger ClearSCADA systems with more than two clients.

Systems running on desktop hardware should run desktop operating systems such as Windows 7, Windows Vista, or Windows XP. Desktop operating systems are designed for user interaction on the computer on which they are installed.

Desktop operating systems should not be used for servers with more than two clients as the TCP/IP security measures in these operating systems can cause significant delays.


32 Bit



ClearSCADA can be installed on computers using the following operating systems:

Server Hardware



Windows Server 2008 R2 (Standard and Enterprise editions) - initial release
Windows Server 2008 (Standard and Enterprise editions) - initial release/Service Pack 1
Windows Server 2003 (Standard and Enterprise editions) - Service Pack 1/Release 2 and Service Pack 2
Windows 2000 Server - Service Pack 4.

Desktop Hardware



Windows 7 (Ultimate and Professional editions) - initial release
Windows Vista (Ultimate and Business editions) - initial release, Service Pack 1 and Service Pack 2
Windows XP (Professional Edition) - Service Pack 2 (including 2a, 2b, and 2c) and Service Pack 3.

ClearSCADA also requires Internet Explorer 6, 7 or 8. Other browsers are not supported.

Crystal Reports XI Release 2 is not supported by the vendor on Windows Server 2008 or Windows Server 2008 R2. For users with installed Server 2008 or Server 2008 R2 systems, it is recommended that the Crystal development application is installed on a Server that is NOT running Windows Server 2008 or Windows Server 2008 R2.


64 Bit



ClearSCADA can be installed on computers using the following operating systems:

Server Hardware



Windows Server 2008 R2 (Standard and Enterprise editions) - initial release
Windows Server 2008 (Standard and Enterprise editions) - initial release/Service Pack 1
Windows Server 2003 (Standard and Enterprise editions) - Service Pack 1/Release 2 and Service Pack 2

Desktop Hardware



Windows 7 (Ultimate and Professional Editions) - initial release
Windows Vista (Ultimate and Business editions) - initial release, Service Pack 1 and Service Pack 2

ClearSCADA also requires Internet Explorer 6, 7 or 8. Other browsers are not supported.

Crystal Reports XI Release 2 is not supported by the vendor on Windows Server 2008 or Windows Server 2008 R2. For users with installed Server 2008 or Server 2008 R2 systems, it is recommended that the Crystal development application is installed on a Server that is NOT running Windows Server 2008 or Windows Server 2008 R2.


Go: Home Back

Author

Biography

Anonymous user

Link copied. Please paste this link to share this article on your social media post.

  • Back to Blog
  • Newer Article
  • Older Article
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.