Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hi team,
Need your support for...
Physical connection: The Panel Server PASS600 is connected to several wired and wireless third-party devices and Schneider 1130 energy meters via RS485 and Ethernet (Modbus). My Modbus master is connected to the PASS600 and is able to pull data from those devices through the assigned virtual server ID of the PASS600.
Issue: Currently, I am able to read the diagnosis data for each wireless device (PER, RSSI, LQI) from my Modbus master using Modbus register 31145, etc. (refer to the file “DOCA0241EN-10”). However, this document does not include any Modbus register for diagnosis data related to Modbus serial and Ethernet devices.
Requirement: I would like to read the diagnosis data for each Modbus serial and Ethernet device, which is already available in the PASS600 web interface under the Maintenance tab. For example:
Please share the Modbus register addresses to read the diagnosis data.
Link copied. Please paste this link to share this article on your social media post.
Hello @Santhoshhedya
What you are referring to is Wireless KPI for zigbee devices (PER, LQI, RSSI), this is available today through modbus.
Regarding modbus protocol as far as I know it is only available in the diagnosis communication pages in Web pages. For serial modbus devices exception codes are not detailed, you need to check the full log for details.
Kind Regards
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
I need Modbus registers to read and write the marked diagnosis data of PAS600.for connected devices to PAS600.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hi Guillaume_Evrard ,
Could you confirm if there are existing models or features available that support this? Or, can we expect such functionality to be included in an upcoming firmware release for the PAS600?
Because, We are planning to use the PAS600 (around 100 no's ) and need a solution to monitor the communication status for all our field devices.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.