Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84375members
353559posts

Logging data from Meter using EGX or using Designer

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Parlindungan_Sitorus
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
3
139

Logging data from Meter using EGX or using Designer

Dear All,

I have a question:

Is there any different between logging data from meter using EGX and if I logging data from the same meter using Designer on PME 7.2?

Thank you.

3 Replies 3
GENJUA
Lt. Commander
Lt. Commander
0 Likes
2
72

Re: Logging data from Meter using EGX or using Designer

I assume that at the top front level software is PME 7.2 , Now if you wish to logs data from EGX means you have to define the meter in management console, and in designer we usually/most of the times deal with the meters which are already defined in the management console.

I might give you more enhance and clear answer if you share more details that what you are trying to achieve.

Thank You,

Parlindungan_Sitorus
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
72

Re: Logging data from Meter using EGX or using Designer

I just suspect, because I see there is a big difference in value between energy usage in incoming and summation of outgoing in the feeder. The meter which is used in incoming are PM810 and are logged in PME v.7.2.2, while in the outgoing feeder are ION6200 and are not logged in PME v.7.2.2 directly. So I made a log function in designer so that ION6200 meters can be logged.

Or, What else factor that could make this happened?

Thank you.

GENJUA
Lt. Commander
Lt. Commander
0 Likes
0
72

Re: Logging data from Meter using EGX or using Designer

any particular reason that you are not logging ION6200 directly into PME 7.2?

For me life can be easy if i start logging ION6200 as well,