Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Hello,
I have a device connected to a link150 using RS485. I would like to emulate a Com port on my laptop to connect to the device.
The tool needs to allow me to enter IP address and slave device ID.
Do you have a handy tool ?
Thanking in advance,
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Thanks a lot Randi, but is it possible to use modsim to act as a virtual com port ?
I would like to use easergypro on my laptop to connect to serial port of protection relay through a link150.
Easergy pro does not allow to enter the slave ID of the relay....
Link copied. Please paste this link to share this article on your social media post.
I'm not aware of any software solution to be used with Link150, but I think that MOXA's NPort device could be what you are looking for.
Link copied. Please paste this link to share this article on your social media post.
Bonjour,
cela fait des années que l'on utilise Modscan32 et on n'a encore rien trouvé de mieux ni d'aussi simple et rapide.
Link copied. Please paste this link to share this article on your social media post.
Bonjour,
Comment fais-tu pour pouvoir avoir modscan32 = Com port Virtuel ?
Mon but est d'aller chercher un équipement connecté en série avec un logiciel qui ne permet pas d'entrer une adresse IP et un esclave modbus....
Link copied. Please paste this link to share this article on your social media post.
Il faut configurer les IP sur la Link150 et dans modscan.
Configurer également la partie Modbus, par défaut on met 19200 8 bits 1 stop Even 0,5sec
sur la photo c'est un exemple pour lire une valeur sur un IM400.
Au passage cela nous arrive de faire une formation à Rennes sur quelques basiques de la communication des équipements, pour des Schneider et des clients, cela dure une journée; (en support on utilise des TGBT Okken)
Link copied. Please paste this link to share this article on your social media post.
Hello @sesa157458_brid ,
For use with eSetup Easergy Pro => I do not think this is possible.
Documentation is not mentioning this option:
Not sure you can commission P3 or P5 through Link150. You can do some setup but only with the Web Pages of the device.
For P3 + eSetup EasergyPro => only through front face (COM port of your Laptop) or direct Ethernet.
Better ask here:
https://community.se.com/t5/PAE-Protection-Relays-Controllers/bd-p/energy-automation
Regards,
Link copied. Please paste this link to share this article on your social media post.
Merci mais ce n'est pas mon besoin, et je connais modpoll, modscan....
Link copied. Please paste this link to share this article on your social media post.
In this case this a P1 and you can have Modbus S1 that seems modbus.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.