Gateways and Energy Servers
Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
User | Count |
---|---|
82 | |
46 | |
29 | |
28 |
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Actually, I'm the one that should be apologizing. I thought you were asking if you could use both of the serial ports (there is a RJ-45 connector and a terminal connector).
Yes, you can most definitely use both the Ethernet and the serial port at the same time 🙂
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Hi,
Technically, both ports could be used, since they are electrically connected in parallel. However, special care needs to be taken to ensure that the wiring polarization is not reversed on the terminal connector. Also, the baud rate and parity needs to be the same for the devices on both ports.
This is possible, but could be tricky.
Randi
Link copied. Please paste this link to share this article on your social media post.
Sorry, I didnt understand very well. Do I have to modify the Ethernet Baud Rate in order to coincide with the serial baud rate? Here is the communication architecture
Link copied. Please paste this link to share this article on your social media post.
Actually, I'm the one that should be apologizing. I thought you were asking if you could use both of the serial ports (there is a RJ-45 connector and a terminal connector).
Yes, you can most definitely use both the Ethernet and the serial port at the same time 🙂
Best regards,
Randi
Link copied. Please paste this link to share this article on your social media post.
Thank you Randi.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Hello @p_dejarmy_encos
I configured the ethernet ports as "2 Switched Ports (1 IP address for both)", the ComX510 is in the same network with the PM5560s, then I confirmed Pin and add the PM5560
I hope It helps
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.