Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

COM'x 200 Publishing all device readings in one CSV file

Gateways and Energy Servers

Schneider Electric support forum to share knowledge about product selection, installation and troubleshooting for EcoStruxure Panel Server, PowerTag, Com'X, Link150…
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
  • EcoStruxure Power & Grid
  • Gateways and Energy Servers
  • Re: COM'x 200 Publishing all device readings in one CSV file
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Romain_Polette
Romain_Polette Champion
125
Guillaume_Evrard
Guillaume_Evrard Leader
59
Randi_Dolan
Randi_Dolan Leader
46
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Gateways and Energy Servers
Start a Topic
Solved
sean-harkin
sean-harkin
Explorer

Posted: ‎2020-01-27 08:07 AM

0 Likes
8
2248
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
‎2020-01-27 08:07 AM

COM'x 200 Publishing all device readings in one CSV file

Hi

 

I am wondering if there is a way through the Publishing in the Com'x 200 to instead of creating one .CSV file per device to publish to an FTP server, you could create one .CSV file with all the required data from the meters. The project that the devices will be used on will contain a large number of meters so creating reports for all them would prove to be unwieldy for this. 

Any help on if this is possible or not would be appreciated.

 

Thanks

Sean

Tags (3)
  • Tags:
  • com'x
  • com'x 200
  • com'x200
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Randi_Dolan
Randi_Dolan Leader
Leader

Posted: ‎2020-01-27 09:57 AM

0 Likes
7
2244
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
‎2020-01-27 09:57 AM

Hi Sean,

 

Unfortunately, the Com'X 200 does not have a method to publish all of the device readings in one CSV file.  Also, the Com'X200 is no longer in development.  So, no changes are being made to this device.

 

Regards,

Randi

See Answer In Context

Reply
Replies 8
Randi_Dolan
Randi_Dolan Leader
Leader

Posted: ‎2020-01-27 09:57 AM

0 Likes
7
2245
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
‎2020-01-27 09:57 AM

Hi Sean,

 

Unfortunately, the Com'X 200 does not have a method to publish all of the device readings in one CSV file.  Also, the Com'X200 is no longer in development.  So, no changes are being made to this device.

 

Regards,

Randi

Reply
sean-harkin
sean-harkin
Explorer

Posted: ‎2020-01-28 12:12 AM

0 Likes
0
2241
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
‎2020-01-28 12:12 AM

Thanks for the update, Randi

 

Regards

Sean

Reply
sean-harkin
sean-harkin
Explorer

Posted: ‎2020-01-28 02:37 AM

0 Likes
5
2239
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
‎2020-01-28 02:37 AM

Just as a follow up to this, would this be possible to achieve on a Com'x 210?

Reply
Randi_Dolan
Randi_Dolan Leader
Leader

Posted: ‎2020-01-28 06:01 AM

0 Likes
4
2235
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
‎2020-01-28 06:01 AM

I can put it in as a feature request. 🙂

Reply
sean-harkin
sean-harkin
Explorer

Posted: ‎2020-01-28 07:07 AM

0 Likes
3
2232
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
‎2020-01-28 07:07 AM

Thanks for that. How long does it usually take to get feedback on the request

Reply
Randi_Dolan
Randi_Dolan Leader
Leader

Posted: ‎2020-01-28 07:13 AM

0 Likes
2
2230
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
‎2020-01-28 07:13 AM

I brought it up in our meeting this morning and it seems highly unlikely that this feature will be implemented, since this device is nearing the end of it's development.  However, I've logged it for the offer manager to consider.  One "objection" that was raised stemmed around the potential size of this file and that email servers limit the size of attachments.  Regardless, it will, at least, be considered at our next increment planning, which is in late March.

Reply
sean-harkin
sean-harkin
Explorer

Posted: ‎2020-01-29 01:52 AM

0 Likes
1
2225
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
‎2020-01-29 01:52 AM

Hi

 

You mentioned that the device is nearing the end of it's development for the Com'x 210. Just for clarification would that mean that the support for the device will be ending or if the device itself is being discontinued and what would be the time frame then for the end of it's development

 

Thanks

Sean

Reply
Randi_Dolan
Randi_Dolan Leader
Leader

Posted: ‎2020-01-29 06:14 AM

0 Likes
0
2221
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
‎2020-01-29 06:14 AM

Support for the Com'X 200/210/510 will continue for several years.  However, development on this device is slated to end at the end of 2020.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.