Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey

Gateway FAQ

Answers to common questions about the EcoStruxure IT Gateway
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • Gateway
  • Gateway FAQ
Options
  • My Knowledge Base Contributions
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support

Gateway FAQ

Sort by:
Helpfulness
  • Date
  • Views
  • Likes
  • Comments
  • Helpfulness
Options
  • Subscribe
  • Bookmark
  • Invite a Friend
  • « Previous
    • 1
    • 2
  • Next »

Do I need a dedicated server for EcoStruxure IT Gateway?

It is recommended that you install EcoStruxure IT Gateway on a dedicated VM or hardware server. If you must install the Gateway on a server with shared resources, make sure there are enough free resources for your Gateway installation. The required CPU and memory depends on the number of monitored devices and the protocol. See System requirements for EcoStruxure IT Gateway EcoStruxure IT Gateway security considerations
View full article
Picard EcoStruxureIT
‎2022-08-18 01:37 AM

7287 Views

Can the Gateway discover SmartConnect UPSs?

Yes. The EcoStruxure IT Gateway can discover APC EcoStruxure Ready Smart-UPS that use a Network Management Card via SNMPv1 or SNMPv3. You also can connect your EcoStruxure Ready Smart-UPS directly to EcoStruxure IT using the SmartConnect port. Features are limited. See Discovering EcoStruxure Ready Smart-UPS in the Gateway See Monitoring APC Smart-UPS with SmartConnect in EcoStruxure IT
View full article
Picard EcoStruxureIT
‎2019-06-04 01:25 AM

1368 Views

Can I change the default subnet for the Gateway appliance private LAN?

Gateway appliance version 1.10 and newer Yes. You can change the default settings from the Gateway appliance private network user interface. See EcoStruxure IT Gateway appliance installation and setup - version 1.10 and newer Gateway appliance version 1.9 and older No. The Gateway appliance private LAN subnet must be 198.168.x.x. The IP address for the Gateway appliance is 192.168.0.1 by default. You must contact support to change the Gateway appliance private LAN subnet to anything other than 192.168.x.x. DO NOT USE WEBMIN TO CHANGE THE SUBNET FOR THE GATEWAY APPLIANCE PRIVATE LAN  If you connect to Webmin on the private LAN and change the Gateway appliance IP address to a subnet other than 192.168.x.x, you will be locked out of Webmin, and completely locked out of the Gateway appliance. You must then call support to reset your appliance.
View full article
Picard EcoStruxureIT
‎2019-10-11 04:40 AM

1384 Views

Can EcoStruxure IT Gateway discover devices on the DCE private LAN?

Both the EcoStruxure IT Gateway software installed on a server and the EcoStruxure IT Gateway appliance can be used to monitor devices across multiple network interfaces. This includes incorporating the Gateway into an existing DCE deployment to monitor devices on the DCE private LAN.  Gateway appliance The Gateway Appliance has dual network ports. It can be used exclusively on the public network connection, or also be connected to a secondary private network. The Gateway appliance includes DHCP server functionality on the secondary network, similar to the DCE server. There must be only one DHCP source a given network. If you connect the Gateway appliance's secondary network to a network that is already serviced by a DHCP source, be sure to follow the documentation on Managing DHCP on the Gateway appliance to disable the Gateway appliance's DHCP server.  Installed Gateway software The Gateway can discover equipment connected to any of the network adapters on the system running the Gateway software. The installed Gateway software does not provide DHCP server functionality. If your private network has no DHCP source, you must install and configure a DHCP server on that subnet. If you need to add an additional network adapter to a system that is already running the Gateway, you must restart the Gateway software before the new adapter will be recognized by the software.
View full article
Picard EcoStruxureIT
‎2020-11-30 07:41 AM

1835 Views
  • « Previous
    • 1
    • 2
  • Next »
Didn't find what you are looking for? Ask our Experts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.