Posted: 2020-07-03 09:42 PM . Last Modified: 2024-04-07 11:40 PM
dce 7.4.3 client and windows 10 compatibility
Is the DCE 7.4.3 client compatible with windows 10? I recently upgraded my os to windows 10, when I went to reinstall the DCE client, the installation failed with the following error.
(CID:123347706)
- Labels:
-
Data Center Expert
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
Posted: 2020-07-03 09:42 PM . Last Modified: 2024-04-07 11:40 PM
Hi jmeza,
Yes, of course, DCE-client is fully compatible with MS Windows 10 (x86 and x64).
At me, for example, the DCE-client is normally installed on MS Windows 10 Home x64.
Please specify the full name of the installation file that you are trying to install in your MS Windows 10?
With respect.
(CID:123347764)
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
Posted: 2020-07-03 09:42 PM . Last Modified: 2024-04-07 11:40 PM
Hi jmeza,
Have you solved this problem or not?
With respect.
(CID:123348038)
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
Posted: 2020-07-03 09:42 PM . Last Modified: 2024-04-07 11:40 PM
Hi jmeza,
I'm assuming your issue was solved. If not, please ask another question.
Thanks,
Stine
(CID:128747691)
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
Posted: 2020-07-03 09:42 PM . Last Modified: 2023-10-22 04:29 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.