Posted: 2020-07-05 05:22 PM . Last Modified: 2024-04-03 03:23 AM
Upgrade DCO from version 8.0.1 to 8.2.7 or 8.2.12
Hello
How I can upgrade DCO from version 8.0.1 to 8.2.12 or 8.2.7 in one hope ?
Will this upgrade work from WebMin Upgrade option ?
(CID:140219629)
- Labels:
-
Data Center Operation
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2024-04-03 03:23 AM
Hello Boris.
This upgrade is supported.
Does your DCO server have access to the public internet?
There have been some reported problems when upgrading from earlier 8.0.x, 8.1.x, and early 8.2.x releases to newer DCO versions like 8.2.7 and 8.2.12 when the DCO server does not have internet access.
If you need to upgrade, make sure you have a backup of your server before the upgrade. Download it off the dco server.
An alternate solution would be to create a backup, download it from the dco server, cold/fresh install DCO 8.2.12 on the server, then restore the backup from the earlier DCO release.
In either case there were also changes to the DCO database between DCO 8.0.x and 8.2.7 and 8.2.12 which means the database upgrade steps are run after the DCO application portion of the upgrade occurs, which means it may take longer than usual for DCO services to completely restart after this upgrade.
Regards
Greg Sterling
(CID:140220122)
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2024-04-03 03:23 AM
Hello Greg
Unfortunately the DCO that I'll go to update haven't access to internet .
In indefinitely this is installation is REDHAT + Install dco , no CentOS
(CID:140707492)
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2024-04-03 03:23 AM
Hello Boris.
My suggestion would be to take a backup of your current running system, download it from DCO server and do a fresh/clean install of DCO 8.2.12 on a new DCO server, then you can restore backup you have downloaded from previous version.
Regards
Elvedin
(CID:140707604)
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2024-04-03 03:23 AM
Hello
What is link to download DCO client version 8.2.12
(CID:140710237)
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2024-04-03 03:23 AM
Hello Boris
You can download desktop clients from Webclient when you have installed DCO.
Regards
Elvedin
(CID:140710239)
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
Posted: 2020-07-05 05:23 PM . Last Modified: 2023-10-22 04:12 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.