EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:32 PM . Last Modified: β2024-04-08 12:56 AM
Hi,
after upgrading UPS (Smart-UPS RT 2000 RM XL) firmware from v6.4.0 to v6.4.6 via DCE (7.4.1.5) and after via FW_Upgrade_R2 tool, the DCE shows this error message: " Device status may be inaccurate because an attempt to transfer a device definition file (DDF) failed."
To be noted that via SSH/console the UPS seems to be ok: AOS and APP both upgraded to v6.4.6 and Stat: P+ N+ A+.
If "upgrading firmware files" were transferred properly, than this mean that this DCE error messages does not depend to scp, ssh, snmp, account and password.
Please advice.
Brgds,
Massimo
(CID:116925087)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2024-04-08 12:56 AM
Hi Massimo,
K-base FA177004 talks about this issue. If you have used the firmware utility (as you mentioned, FW_Upgrade_R2 tool) for the upgrade, there is nothing here proving that SSH/SCP between DCE and the device are not having issues. DCE may not have the right settings or passwords. The network can also be blocking the correct protocol between the server and device while allowing it from the computer you used the FW_Upgrade_R2 tool on.
If you check the release notes however, you will see the following under known issues on the recent DCE versions
Β· APC SNMP Device Configuration File Transfer Using SCP Fails
File transfer using SCP fails on some APC SNMP devices with firmware lower than AOS v6.3.3. For best results, enable FTP on the device, and set the protocol to FTP Only in the βDevice File Transfer Settingsβ display before you select the devices you want to update. Additionally, both SCP and FTP file transfer fails on all v6.x devices with touch screens (apc_hw06_aos_xxx). See the StruxureWare Data Center Expert documentation on http://dcimsupport.apc.com for the most recent information on APC SNMP Device Configuration.
Steve
(CID:116925100)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2024-04-08 12:56 AM
Ciao Steven,
just finished to do some test:
so the cause of problem seems to be the "Apply Firmware Update..." features of DCE using "scp only" as transfer method.
Brgds,
Massimo
(CID:116925335)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2024-04-08 12:55 AM
... Just noted that DCE v7.4.3 should solve DDF problems.
I've just requested this version.
NOTE: After a while also the second UPS showed the same problem.
brgds,
Massimo.
(CID:116925337)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2024-04-08 12:55 AM
Not sure if this is the case in your scenario but we have a few of our devices Firewalled and in order to get SCP to work we have to allow PING protocol. Looks like it pings the device first and if it gets a response it continues but if it gets no response then it fails. just a thought...
Toby
(CID:116926385)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2024-04-08 12:55 AM
Toby Bouzane, of course, is right about the ICMP-protocol, which is used, in particular, for the ping command.
After all, as far as I know, both the FW_Upgrade_R2 tool under MS Windows and the built-in device firmware update tools in the DCE-server operate the above protocol to determine the availability of devices after consecutive reboots (after the apc bootmon, apc aos and apc app components are updated).
With best regards.
(CID:116926434)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 03:33 PM . Last Modified: β2023-10-22 04:08 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.