EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:54 PM . Last Modified: 2024-04-08 01:09 AM
Hi all!
In continuation of the topic discussed in the I want to ask some questions on the installation of the above software in the OS environment RHEL/CentOS-7.x.
Q1: If you follow Installing IT Optimize instruction, then the Schneider Electric IT Optimize software is installed, namely the energycenter component. This can also be checked by successfully visiting the link, for example https://localhost:8090. But the components of Intel DCM and Intel KVM (which are present in the installation tarball StruxureWareItOptimizeWithServerAccess-setup-7.5.2.linux.x64.tar.gz) are not installed in this case, which can be easily checked for inaccessible links, for example, http://localhost:8688/DataCenterManager/ (or https://localhost:8643/DataCenterManager/). So how do you properly install the above software?
Q2: This is not even a question, but a remark about the problem. If you perform a subsequent uninstallation of SxW ITO, the associated processes mysql and java for some reason do not stop and do not kill. In addition, the viridity user and his home directory are not removed from the system. As a result, if you do not pay attention to this and then try to reinstall SxW ITO, the installer already invisibly suggests for the ITOptimize Web Application Port Setting not the default port of 8090, but 8091. And this moment can be ignored and then unsuccessfully try to login on port 8090, as indicated in the instructions 😀.
Very thanks for the support.
(CID:116364138)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:55 PM . Last Modified: 2024-04-08 01:09 AM
Hello @spezialist
I will make sure our documentation for installation of ITO on the modern CentOS / RH is updated to include the following.
(CID:116921091)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:54 PM . Last Modified: 2024-04-08 01:09 AM
Hi spezialist,
thanks for posting. Lets see who can be of assistance here. @community any ideas?
Kind regards Ditte
(CID:116364986)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:55 PM . Last Modified: 2024-04-08 01:09 AM
Hello @spezialist
I will make sure our documentation for installation of ITO on the modern CentOS / RH is updated to include the following.
(CID:116921091)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:55 PM . Last Modified: 2024-04-08 01:09 AM
Hi Greg Sterling,
Thank you very much for the short manual: it is very useful.
My mistake was that I made only one *.bin file executable. As soon as I made all *.sh files executable, the problem was solved 😀. The ITO-software was installed normally in its entirety.
Greg Sterling convert your comment to answer and I mark it as solved.
Very thanks for the support.
(CID:116921093)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2020-07-03 02:55 PM . Last Modified: 2023-10-22 04:04 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.