Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82449members
349995posts

Rocky linux package

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Jerome_C
Ensign
Ensign

Rocky linux package

Hi,

 

Recently, the last update of  DCE and IT Advisor migrate from CentOS to Rocky Linux.

Would it be possible to provide the zabbix-agent and qemu-guest-agent package with the Rocky Linux distribution so we can have a better integration in our virtual infrastructure ?

 

Kind regards,

 

Jerome 

 

Tags (1)
2 Replies 2
gsterling
Commander Commander
Commander
0 Likes
1
251

Re: Rocky linux package

Hello Jerome

 

Responding at a high level.

 

DCE is provided in the form of an appliance. Customers do not in general have access to the operating system thus modules which are not essential to the functioning DCE software cannot be installed. Even if it were installed, its unlikely you'd have access to the modules and their features as OS level access is not provided.

 

For ITA, customers may deploy their own Redhat 8.x or Rocky Linux 8.x OS (CentOS 8.x if ITA is a 9.x release prior to 9.3.0). Customers are permitted to install other tools and modules as they need as long as those tools do not interfere with the IT Advisor application. We have a number of customers who deploy their own malware tools, log collection or backups tools on their ITA server. So you are free to install the tools you mention as long as they do not break IT Advisor.

 

As a policy for ITA, Schneider tries to offer the modules needed for general use of IT Advisor so we do not usually include third party modules like the ones you specified

 

Regards

 

Greg Sterling

Tags (1)
Jerome_C
Ensign
Ensign
0 Likes
0
185

Re: Rocky linux package

Hi,

 

Thank you for the reply Gregory !

Well i guess, i knew the answer before i post my request.

I am sure, i am not the only one interested with the such features as every virtual platform has his own tools/agent which (should) improve the integration and the monitoring.

I know it is difficult regarding the support contract policy but on the other hand you could also have some interesting and valuable feedback from customers which use different virtual infrastructure.

 

Kind regards,

 

Jerome

 

 

Tags (1)