EcoStruxure IT forum
Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:06 AM . Last Modified: β2024-04-08 03:39 AM
Hello,
I have updated the firmware on four of my PDUS but two have hung (for days) with the message Waiting for RPDU2G 6.4.4 to load....
The PDUS are both AP8653 models
I have rebooted the management server and the pdus.
If i launch directly to the pdu i see that its running 6.4.4.
How can i update the firmware update page to show these puds as being upgraded?
Thanks
Patrick
(CID:110008131)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:39 AM
Not an expert here but wanted to suggest some things:
Have you verified the SNMP settings, username/password DCE uses and also right click on the device and click "Request Device Scan".
If the device is updated, I would like DCE should notice that in a few minutes but it sounds like DCE isn't getting a response back from the device.
Do you get alarms? trends?
Regards,
J
(CID:110008149)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:39 AM
I dont have any alarms configured but if i setup a report it can retrieve the data which I thought used SNMP.
(CID:110008152)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:39 AM
Hi Patrick,
It looks like DCE is simply stuck looking to verify the version of firmware. What version of DCE are you using?
The first thing I would suggest is to reboot the server.
I'd also be curious to know if you went back to the firmware upgrade page (where you initiated the upgrade of the PDUs), does it show the correct firmware or is it prompting you to be able to upgrade the firmware again?
Is it just these 2 PDUs? Do you have others that worked?
Thanks,
Steve
(CID:110008168)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:39 AM
Hi Steve, I have already rebooted the server and the management interfaces of the PDUs. it shows the PDU as running app and os version 6.4.4, if I logon to the PDU it also says its running 6.4.4. The management server is running Client Build: 7.4.1.5 and Server Build: 7.4.1.5. there are two other PDUs in the same segment that updated fine. Regards Patrick
(CID:110008450)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:38 AM
I ended up deleting and recreating the two offending PDUs.
(CID:110008516)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2024-04-08 03:38 AM
Sorry to hear that. I knew that would resolve it but that causes the loss of historrical data and I would hope there would have been a less intrusive resolution. Thanks for the update Steve
(CID:110008519)
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: β2020-07-03 09:07 AM . Last Modified: β2023-10-22 03:30 AM
This question is closed for comments. You're welcome to start a new topic if you have further comments on this issue.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.