Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84757members
354188posts

Ortea Sirus Stabilizer Keeps Changing MAC Address

EcoStruxure IT forum

A support forum for Data Center Operation, Data Center Expert, and EcoStruxure IT product users to share knowledge on installation, configuration, and general product use.

Solved
Angwenyi
Ensign
Ensign
0 Likes
2
510

Ortea Sirus Stabilizer Keeps Changing MAC Address

Dear Team,

 

We have a customer with subject unit, we've connected it to the DCE via Modbus over IP.

 

However, customer claims it keeps getting blacklisted due to changing MAC address.

 

I have never heard units changing MAC address on the TCP/IP environment, anyone know if this is a issue with Modbus over IP.

 

Thank you.

 

Regards,

 

Felix

Tags (1)

Accepted Solutions
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
497

Re: Ortea Sirus Stabilizer Keeps Changing MAC Address

Hi,

 

If the mac address of the Ortea device keeps changing, I would suggest this should probably be taken up with Ortea.

 

This shouldn't affect modbus specifically, but it will affect how the rest of the network gets requests to and from the device in the first place - and "blacklisted" makes it sound like they have some network security in place that the changes really don't play well with.

 

If it's the mac address of the DCE that's changing, something's gone very wrong - the DCE really doesn't like its address being changed, so this would cause huge issues.

See Answer In Context

Tags (1)
2 Replies 2
Shaun
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
498

Re: Ortea Sirus Stabilizer Keeps Changing MAC Address

Hi,

 

If the mac address of the Ortea device keeps changing, I would suggest this should probably be taken up with Ortea.

 

This shouldn't affect modbus specifically, but it will affect how the rest of the network gets requests to and from the device in the first place - and "blacklisted" makes it sound like they have some network security in place that the changes really don't play well with.

 

If it's the mac address of the DCE that's changing, something's gone very wrong - the DCE really doesn't like its address being changed, so this would cause huge issues.

Tags (1)
Angwenyi
Ensign
Ensign
0 Likes
0
375

Re: Ortea Sirus Stabilizer Keeps Changing MAC Address

Hi Shaun,

 

Thank you for your prompt response.

Tags (1)